<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K396和S32K376是否pin to pin兼容 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1895734#M36992</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;S32K396评估板文件包&lt;EM&gt;&lt;SPAN&gt;S32K396BMS-EVB-DESIGN-FILES.zip&lt;/SPAN&gt;&lt;/EM&gt;中，电路设计是基于&lt;SPAN&gt;S32K396&lt;/SPAN&gt;，请问是否可以直接将&lt;SPAN&gt;MCU&lt;/SPAN&gt;替换为&lt;SPAN&gt;S32K376&lt;/SPAN&gt;？或需要进行怎样的改动？&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;In the s32K396 evaluation board file package S32K396BMS-EVB-DESIGN-FILES.zip, the circuit design is based on S32K396, can I directly replace the MCU with S32K376?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; Or what changes need to be made?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jun 2024 07:22:04 GMT</pubDate>
    <dc:creator>chenhuang</dc:creator>
    <dc:date>2024-06-28T07:22:04Z</dc:date>
    <item>
      <title>S32K396和S32K376是pin to pin兼容吗？</title>
      <link>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1895556#M36984</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;请问S32K396和S32K376是pin to pin兼容吗？RM手册附件的IO 相关资料全都是S32K396的描述;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Are S32K396 and S32K376 Pin-to-PIN compatible?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; The IO related materials attached to the RM manual are all descriptions of S32K396;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 02:57:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1895556#M36984</guid>
      <dc:creator>chenhuang</dc:creator>
      <dc:date>2024-06-28T02:57:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K396和S32K376是否pin to pin兼容</title>
      <link>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1895734#M36992</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;S32K396评估板文件包&lt;EM&gt;&lt;SPAN&gt;S32K396BMS-EVB-DESIGN-FILES.zip&lt;/SPAN&gt;&lt;/EM&gt;中，电路设计是基于&lt;SPAN&gt;S32K396&lt;/SPAN&gt;，请问是否可以直接将&lt;SPAN&gt;MCU&lt;/SPAN&gt;替换为&lt;SPAN&gt;S32K376&lt;/SPAN&gt;？或需要进行怎样的改动？&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;In the s32K396 evaluation board file package S32K396BMS-EVB-DESIGN-FILES.zip, the circuit design is based on S32K396, can I directly replace the MCU with S32K376?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; Or what changes need to be made?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 07:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1895734#M36992</guid>
      <dc:creator>chenhuang</dc:creator>
      <dc:date>2024-06-28T07:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K396和S32K376是pin to pin兼容吗？</title>
      <link>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1896128#M37018</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203108"&gt;@chenhuang&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, they are software and pin-compatible.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 22:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1896128#M37018</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-06-28T22:37:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K396和S32K376是pin to pin兼容吗？</title>
      <link>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1896173#M37020</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Julián ，&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have understood, thank you for your support;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 29 Jun 2024 02:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K396%E5%92%8CS32K376%E6%98%AFpin-to-pin%E5%85%BC%E5%AE%B9%E5%90%97/m-p/1896173#M37020</guid>
      <dc:creator>chenhuang</dc:creator>
      <dc:date>2024-06-29T02:44:57Z</dc:date>
    </item>
  </channel>
</rss>