<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3xx: Standby Mode &amp;amp; Wake Pin Query in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-Standby-Mode-amp-Wake-Pin-Query/m-p/1895176#M36970</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a query regarding the S32K3xx (specifically) for S32K312 controllers.&lt;/P&gt;&lt;P&gt;In Standby mode, I would like to wake up the controller using an external GPIO signal. I am planning to use the WAKE Pins for this purpose.&lt;/P&gt;&lt;P&gt;As per the S32K3 Datasheet, there are 3 standby modes of the S32K3xx:&lt;BR /&gt;1) Standby with All OFF&lt;BR /&gt;2) Standby with SIRC ON&lt;BR /&gt;3) Standby with FIRC ON&lt;BR /&gt;&lt;BR /&gt;I have the following queries (wrt S32K312) :&lt;BR /&gt;&lt;STRONG&gt;Q1)&lt;/STRONG&gt; How does the controller come out of the standby mode in the case of "Standby with All OFF" mode.&lt;BR /&gt;&lt;STRONG&gt;Q2)&lt;/STRONG&gt; Can I use the "Standby with SIRC ON" mode if I want the controller to come out of standby using external Wake pins?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Any inputs on the above queries will be of help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jun 2024 13:08:37 GMT</pubDate>
    <dc:creator>tecprasant</dc:creator>
    <dc:date>2024-06-27T13:08:37Z</dc:date>
    <item>
      <title>S32K3xx: Standby Mode &amp; Wake Pin Query</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-Standby-Mode-amp-Wake-Pin-Query/m-p/1895176#M36970</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a query regarding the S32K3xx (specifically) for S32K312 controllers.&lt;/P&gt;&lt;P&gt;In Standby mode, I would like to wake up the controller using an external GPIO signal. I am planning to use the WAKE Pins for this purpose.&lt;/P&gt;&lt;P&gt;As per the S32K3 Datasheet, there are 3 standby modes of the S32K3xx:&lt;BR /&gt;1) Standby with All OFF&lt;BR /&gt;2) Standby with SIRC ON&lt;BR /&gt;3) Standby with FIRC ON&lt;BR /&gt;&lt;BR /&gt;I have the following queries (wrt S32K312) :&lt;BR /&gt;&lt;STRONG&gt;Q1)&lt;/STRONG&gt; How does the controller come out of the standby mode in the case of "Standby with All OFF" mode.&lt;BR /&gt;&lt;STRONG&gt;Q2)&lt;/STRONG&gt; Can I use the "Standby with SIRC ON" mode if I want the controller to come out of standby using external Wake pins?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Any inputs on the above queries will be of help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 13:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-Standby-Mode-amp-Wake-Pin-Query/m-p/1895176#M36970</guid>
      <dc:creator>tecprasant</dc:creator>
      <dc:date>2024-06-27T13:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx: Standby Mode &amp; Wake Pin Query</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-Standby-Mode-amp-Wake-Pin-Query/m-p/1896144#M37019</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228301"&gt;@tecprasant&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Q1)&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;After Standby mode exit, the following events occur:&lt;BR /&gt;1.A wake-up event arrives.&lt;BR /&gt;2.FIRC starts powering up (if disabled in Standby mode).&lt;BR /&gt;3.PMC starts the transition process to FPM (for example, enables the last-mile regulator and provides V11_RUN supply to the chip).&lt;BR /&gt;4.MC_PCU removes the isolation between Run and Standby domains.&lt;BR /&gt;5.Run domain reset deasserts (asserts on Standby mode entry) and the chip undergoes a functional reset exit sequence for this domain.&lt;BR /&gt;6.The chip enters Run mode of operation.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Q2)&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;Yes.You can use the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724" target="_blank"&gt;S32K3 Low Power Management AN and demos&lt;/A&gt;&amp;nbsp;for reference. Please keep in mind they are based in S32DS 3.4 and RTD 2.0.0.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 23:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-Standby-Mode-amp-Wake-Pin-Query/m-p/1896144#M37019</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-06-28T23:29:19Z</dc:date>
    </item>
  </channel>
</rss>