<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Setting S32K312 PLL then system will reset</title>
    <link>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1895079#M36965</link>
    <description>&lt;P&gt;Please refer to the discussion in&amp;nbsp;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;&lt;A href="https://community.nxp.com/t5/S32K/HSE-PLL-configuration/td-p/1672534" target="_self"&gt;HSE PLL configuration&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jun 2024 10:14:31 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-06-27T10:14:31Z</dc:date>
    <item>
      <title>Setting S32K312 PLL then system will reset</title>
      <link>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1893783#M36902</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;The customer setting S32K312 PLL then system will reset, attached file is the customer sample code.&lt;/P&gt;&lt;P&gt;could you give me some comments?&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;FUNC(void, SYSDAL_APPL_CODE) SysDal_DriverInitZero(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; OsIf_Init(NULL_PTR);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Initialise MCU Driver */&lt;/P&gt;&lt;P&gt;#if (MCU_PRECOMPILE_SUPPORT == STD_ON)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mcu_Init(NULL_PTR);&lt;/P&gt;&lt;P&gt;#else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mcu_Init( &amp;amp;Mcu_Config );&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set the CPU Clock to the PLL */&lt;/P&gt;&lt;P&gt;#if (MCU_INIT_CLOCK == STD_ON)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mcu_InitClock(McuClockSettingConfig_HighPerf);&amp;nbsp; // only do this setting, system will reset every one second.&amp;nbsp;&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;#if(MCU_NO_PLL == STD_OFF)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait until the PLL is locked */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (MCU_PLL_LOCKED != Mcu_GetPllStatus()); //include this setting,&amp;nbsp;system will reset one time only.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Activate the PLL Clock */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mcu_DistributePllClock();&amp;nbsp;//include this setting,&amp;nbsp;system will reset one time only.&lt;/P&gt;&lt;P&gt;#endif/*MCU_NO_PLL == STD_OFF*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Initialize PORT */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Port_Init( &amp;amp;Port_Config );&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set the MCU to RUN mode */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Mcu_SetMode(McuModeSettingConf_Run);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Main Loop&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (;;) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (void)Dio_FlipChannel((Dio_ChannelType)DioConf_DioChannel_View1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 16:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1893783#M36902</guid>
      <dc:creator>Felix_ar</dc:creator>
      <dc:date>2024-06-25T16:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: Setting S32K312 PLL then system will reset</title>
      <link>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1893925#M36910</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please check if it is related to the reasons mentioned in the following discussion:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/If-I-don-t-give-s32k312-delay-the-CAN-stop-during-operation/m-p/1828163/highlight/false#M32968" target="_self"&gt;If I don't give s32k312 delay, the CAN stop during operation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I checked your Clock_Ip_PBcfg.c, and it seems to be caused by it:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;{&lt;BR /&gt;&lt;STRONG&gt;AIPS_SLOW_CLK&lt;/STRONG&gt;,&lt;BR /&gt;&lt;STRONG&gt;4&lt;/STRONG&gt;U,&lt;BR /&gt;{&lt;BR /&gt;0U,&lt;BR /&gt;}&lt;BR /&gt;},&lt;/P&gt;
&lt;P&gt;{&lt;BR /&gt;&lt;STRONG&gt;HSE_CLK&lt;/STRONG&gt;,&lt;BR /&gt;&lt;STRONG&gt;1&lt;/STRONG&gt;U,&lt;BR /&gt;{&lt;BR /&gt;0U,&lt;BR /&gt;}&lt;BR /&gt;},&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 01:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1893925#M36910</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-06-26T01:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: Setting S32K312 PLL then system will reset</title>
      <link>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1894338#M36929</link>
      <description>&lt;P&gt;Hi Robin&lt;/P&gt;&lt;P&gt;Thank for your reply, the system reset problem is fixed.&lt;/P&gt;&lt;P&gt;One more question, &lt;STRONG&gt;S32K3xx_DCF_clients.xlxs&lt;/STRONG&gt; mentions&amp;nbsp;&lt;STRONG&gt;HSE_CLK_MODE_AND_GSKT_CTRL &lt;/STRONG&gt;register can set to 1x then HSE clock can set up to 120MHz, but how to change register setting?&lt;/P&gt;&lt;P&gt;Because I can't find&amp;nbsp;&lt;STRONG&gt;HSE_CLK_MODE_AND_GSKT_CTRL &lt;/STRONG&gt;register in reference manual, I have found related register is&amp;nbsp;&lt;STRONG&gt;HSE_CLK_MODE_OPTION,&lt;/STRONG&gt; but that is read only register.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HSE_CLK.png" style="width: 771px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285846i5C5A196B209A0CA6/image-size/large?v=v2&amp;amp;px=999" role="button" title="HSE_CLK.png" alt="HSE_CLK.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;HSE_CLK.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 10:30:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1894338#M36929</guid>
      <dc:creator>Felix_ar</dc:creator>
      <dc:date>2024-06-26T10:30:18Z</dc:date>
    </item>
    <item>
      <title>Re: Setting S32K312 PLL then system will reset</title>
      <link>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1895079#M36965</link>
      <description>&lt;P&gt;Please refer to the discussion in&amp;nbsp;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;&lt;A href="https://community.nxp.com/t5/S32K/HSE-PLL-configuration/td-p/1672534" target="_self"&gt;HSE PLL configuration&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 10:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Setting-S32K312-PLL-then-system-will-reset/m-p/1895079#M36965</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-06-27T10:14:31Z</dc:date>
    </item>
  </channel>
</rss>