<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Recovering from Secure Boot on S32K3 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Recovering-from-Secure-Boot-on-S32K3/m-p/1894601#M36945</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm currently implementing secure boot on a S32K310. I've got two questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;In case I configure secure boot on an SMR, how can I recover if the code in this SMR becomes corrupted? Do I need to flash with a debug probe the non corrupted firmware again? Is there another way?&lt;/LI&gt;&lt;LI&gt;In case I need to modify the code in the SMR after activating the secure boot (during development typically), can I disable secure boot before updating the code and reconfigure secure boot on the new code?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Benoit&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jun 2024 17:37:23 GMT</pubDate>
    <dc:creator>end48</dc:creator>
    <dc:date>2024-06-26T17:37:23Z</dc:date>
    <item>
      <title>Recovering from Secure Boot on S32K3</title>
      <link>https://community.nxp.com/t5/S32K/Recovering-from-Secure-Boot-on-S32K3/m-p/1894601#M36945</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm currently implementing secure boot on a S32K310. I've got two questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;In case I configure secure boot on an SMR, how can I recover if the code in this SMR becomes corrupted? Do I need to flash with a debug probe the non corrupted firmware again? Is there another way?&lt;/LI&gt;&lt;LI&gt;In case I need to modify the code in the SMR after activating the secure boot (during development typically), can I disable secure boot before updating the code and reconfigure secure boot on the new code?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Benoit&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 17:37:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recovering-from-Secure-Boot-on-S32K3/m-p/1894601#M36945</guid>
      <dc:creator>end48</dc:creator>
      <dc:date>2024-06-26T17:37:23Z</dc:date>
    </item>
    <item>
      <title>Re: Recovering from Secure Boot on S32K3</title>
      <link>https://community.nxp.com/t5/S32K/Recovering-from-Secure-Boot-on-S32K3/m-p/1897490#M37099</link>
      <description>&lt;P&gt;1) You will have to update SMR if possible.&lt;/P&gt;
&lt;P&gt;2) Once the secure boot is enabled, it can't be disabled.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 12:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Recovering-from-Secure-Boot-on-S32K3/m-p/1897490#M37099</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-07-02T12:32:55Z</dc:date>
    </item>
  </channel>
</rss>