<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K344 - DIO Configuration support</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-DIO-Configuration-support/m-p/1893361#M36879</link>
    <description>&lt;P&gt;MBDT DIO example used and working fine. When used to generate other pin, made the same settings as per the example except port and channel ID. It not generating ant error, but it is not generating output. Is there any document which help to use DIO?&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jun 2024 06:40:35 GMT</pubDate>
    <dc:creator>Er_AK</dc:creator>
    <dc:date>2024-06-25T06:40:35Z</dc:date>
    <item>
      <title>S32K344 - DIO Configuration support</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DIO-Configuration-support/m-p/1893361#M36879</link>
      <description>&lt;P&gt;MBDT DIO example used and working fine. When used to generate other pin, made the same settings as per the example except port and channel ID. It not generating ant error, but it is not generating output. Is there any document which help to use DIO?&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 06:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DIO-Configuration-support/m-p/1893361#M36879</guid>
      <dc:creator>Er_AK</dc:creator>
      <dc:date>2024-06-25T06:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 - DIO Configuration support</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-DIO-Configuration-support/m-p/1893409#M36884</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Hmm, the usage is quite simple here. Are you sure you have device package which supports the pin you would like to configure?&lt;/P&gt;
&lt;P&gt;DIO documents are inside the driver package in folder doc.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1719300961481.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285590i3BFA08023411E21C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_0-1719300961481.png" alt="petervlna_0-1719300961481.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_0-1719300961481.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you share more details I can try to generate the code for the requested pin.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 07:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-DIO-Configuration-support/m-p/1893409#M36884</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-06-25T07:36:33Z</dc:date>
    </item>
  </channel>
</rss>