<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Continuous adc conversion for multiple channels using SW Trigger in S32k</title>
    <link>https://community.nxp.com/t5/S32K/Continuous-adc-conversion-for-multiple-channels-using-SW-Trigger/m-p/1892493#M36835</link>
    <description>&lt;P&gt;&lt;A href="mailto:Hi@Guna" target="_blank"&gt;Hi@Guna&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you please tell me the part number you're using? and the SDK and IDE version.&lt;/P&gt;
&lt;P&gt;Aslo please provided me your project and i will help you to check it.&lt;/P&gt;</description>
    <pubDate>Mon, 24 Jun 2024 02:06:17 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2024-06-24T02:06:17Z</dc:date>
    <item>
      <title>Continuous adc conversion for multiple channels using SW Trigger in S32k</title>
      <link>https://community.nxp.com/t5/S32K/Continuous-adc-conversion-for-multiple-channels-using-SW-Trigger/m-p/1892406#M36828</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am currently checking adc using SW trigger. As per my requirement, the SW trigger was working properly by calling AdcStartGroupConversion(). which will be called multiple times in a function. Currently, I have added some more channels to the same group. but this time it is not working; it is converting only once after that it is not, even though if I call AdcStartGroupConversion() multiple times. Also, I have other 2 groups with the same configuration and with SW triggers that are converting multiple times. I'm confused now as to why it is not working as expected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I verified all my configurations with other working groups, which are the same. The major change that I have made is adding two more channels to that group. Any idea what is the reason behind this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 22 Jun 2024 15:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Continuous-adc-conversion-for-multiple-channels-using-SW-Trigger/m-p/1892406#M36828</guid>
      <dc:creator>Guna</dc:creator>
      <dc:date>2024-06-22T15:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: Continuous adc conversion for multiple channels using SW Trigger in S32k</title>
      <link>https://community.nxp.com/t5/S32K/Continuous-adc-conversion-for-multiple-channels-using-SW-Trigger/m-p/1892493#M36835</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Guna" target="_blank"&gt;Hi@Guna&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you please tell me the part number you're using? and the SDK and IDE version.&lt;/P&gt;
&lt;P&gt;Aslo please provided me your project and i will help you to check it.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 02:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Continuous-adc-conversion-for-multiple-channels-using-SW-Trigger/m-p/1892493#M36835</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-06-24T02:06:17Z</dc:date>
    </item>
  </channel>
</rss>