<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 P_FLASH write data in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-P-FLASH-write-data/m-p/857361#M3666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The address 0x190001 is out of Flash address range.&amp;nbsp;I assume that you mean the address 0x19001.&lt;/P&gt;&lt;P&gt;Please, refer to the reference manual rev9. to the section "36.5.11.4 Program Phrase command" in that case.&lt;/P&gt;&lt;P&gt;There can be seen the note "1." under the "Table 36-40. Program Phrase Command FCCOB requirements"&lt;/P&gt;&lt;P&gt;The Flash&lt;SPAN style="font-weight: 400;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="font-weight: 400;"&gt;address&lt;/SPAN&gt;&amp;nbsp;&lt;STRONG&gt;Must be 64-bit aligned (Flash address [2:0] = 000)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if Flash address is not 64-bit aligned the&amp;nbsp;FSTAT[ACCERR] bit is set.&lt;/P&gt;&lt;P&gt;Please, refer to "Table 36-41. Program Phrase command error handling".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2019 15:07:17 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2019-01-24T15:07:17Z</dc:date>
    <item>
      <title>S32K144 P_FLASH write data</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-P-FLASH-write-data/m-p/857360#M3665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I write to P_flash(Address 0x19000, 8 bytes),it can write successfullt.&lt;/P&gt;&lt;P&gt;But when the address is 0x190001, the byte can't be writen.&lt;/P&gt;&lt;P&gt;Why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 06:45:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-P-FLASH-write-data/m-p/857360#M3665</guid>
      <dc:creator>玉敏111田</dc:creator>
      <dc:date>2019-01-24T06:45:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 P_FLASH write data</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-P-FLASH-write-data/m-p/857361#M3666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The address 0x190001 is out of Flash address range.&amp;nbsp;I assume that you mean the address 0x19001.&lt;/P&gt;&lt;P&gt;Please, refer to the reference manual rev9. to the section "36.5.11.4 Program Phrase command" in that case.&lt;/P&gt;&lt;P&gt;There can be seen the note "1." under the "Table 36-40. Program Phrase Command FCCOB requirements"&lt;/P&gt;&lt;P&gt;The Flash&lt;SPAN style="font-weight: 400;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="font-weight: 400;"&gt;address&lt;/SPAN&gt;&amp;nbsp;&lt;STRONG&gt;Must be 64-bit aligned (Flash address [2:0] = 000)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if Flash address is not 64-bit aligned the&amp;nbsp;FSTAT[ACCERR] bit is set.&lt;/P&gt;&lt;P&gt;Please, refer to "Table 36-41. Program Phrase command error handling".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 15:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-P-FLASH-write-data/m-p/857361#M3666</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-01-24T15:07:17Z</dc:date>
    </item>
  </channel>
</rss>