<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About UJA1169 that config NWP via CAN bus in S32K</title>
    <link>https://community.nxp.com/t5/S32K/About-UJA1169-that-config-NWP-via-CAN-bus/m-p/1888653#M36654</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;No, it says that the UJA1169A allows to set a long watchdog period up to 4s so that the microcontroller can quite easily be flashed via the CAN bus, basically without having to consider the integrated watchdog.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jun 2024 10:59:34 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2024-06-17T10:59:34Z</dc:date>
    <item>
      <title>About UJA1169 that config NWP via CAN bus</title>
      <link>https://community.nxp.com/t5/S32K/About-UJA1169-that-config-NWP-via-CAN-bus/m-p/1887838#M36610</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;The following sentence comes from the UJA1169A datasheet:&lt;BR /&gt;【&lt;BR /&gt;2.7 System control and diagnostic features&lt;BR /&gt;Watchdog period selectable between 8 ms and 4s supporting remote flash programming via the CAN bus&lt;BR /&gt;】&lt;/P&gt;&lt;P&gt;Please refer to the attached png file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't understand how to support remote flash programming via the CAN bus?&lt;BR /&gt;Is it means that I can config the NWP(Nominal Watchdog Period of Watchdog control register) via other&amp;nbsp; devices on CAN bus?&lt;BR /&gt;Please help me explain it，thanks！&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Fedora&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 10:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-UJA1169-that-config-NWP-via-CAN-bus/m-p/1887838#M36610</guid>
      <dc:creator>fedora</dc:creator>
      <dc:date>2024-06-14T10:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: About UJA1169 that config NWP via CAN bus</title>
      <link>https://community.nxp.com/t5/S32K/About-UJA1169-that-config-NWP-via-CAN-bus/m-p/1888653#M36654</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;No, it says that the UJA1169A allows to set a long watchdog period up to 4s so that the microcontroller can quite easily be flashed via the CAN bus, basically without having to consider the integrated watchdog.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 10:59:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-UJA1169-that-config-NWP-via-CAN-bus/m-p/1888653#M36654</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-06-17T10:59:34Z</dc:date>
    </item>
    <item>
      <title>Re: About UJA1169 that config NWP via CAN bus</title>
      <link>https://community.nxp.com/t5/S32K/About-UJA1169-that-config-NWP-via-CAN-bus/m-p/1888678#M36656</link>
      <description>&lt;P&gt;Oh, I understand it now.&lt;/P&gt;&lt;P&gt;Setting&amp;nbsp;&lt;SPAN&gt;a long watchdog period&amp;nbsp;that can&amp;nbsp;quite easily&amp;nbsp;upgrade the MCU firmware via the CAN bus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you, Tomas !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Fedora&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 11:34:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-UJA1169-that-config-NWP-via-CAN-bus/m-p/1888678#M36656</guid>
      <dc:creator>fedora</dc:creator>
      <dc:date>2024-06-17T11:34:48Z</dc:date>
    </item>
  </channel>
</rss>