<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: How to specify PEmicro to execute pegdbserver_console.exe -startserver -device=NXP_S32K146F1M0M1</title>
    <link>https://community.nxp.com/t5/S32K/How-to-specify-PEmicro-to-execute-pegdbserver-console-exe/m-p/1887898#M36614</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can specify interface and port when you start pegdbserver_console for example like this:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;pegdbserver_console.exe -startserver -device=NXP_S32K3xx_S32K312 -interface=USBMULTILINK -port=PEMB7D193&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;More commands you can find with&amp;nbsp;pegdbserver_console.exe --help&amp;nbsp; command.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jun 2024 12:29:45 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2024-06-14T12:29:45Z</dc:date>
    <item>
      <title>How to specify PEmicro to execute pegdbserver_console.exe -startserver -device=NXP_S32K146F1M0M11</title>
      <link>https://community.nxp.com/t5/S32K/How-to-specify-PEmicro-to-execute-pegdbserver-console-exe/m-p/1876230#M35883</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I want to do automated testing, with one computer connected to two PEmicro devices. The ports for the two devices are different, they are PE5748112 and PE5750306 respectively, and they are connected to S32K146 and S32K148 boards. How do I specify a particular PEmicro to execute the programming command?I hope this job can be done through the command line.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 09:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-specify-PEmicro-to-execute-pegdbserver-console-exe/m-p/1876230#M35883</guid>
      <dc:creator>Jackey_cj</dc:creator>
      <dc:date>2024-05-28T09:59:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to specify PEmicro to execute pegdbserver_console.exe -startserver -device=NXP_S32K146F1M0M1</title>
      <link>https://community.nxp.com/t5/S32K/How-to-specify-PEmicro-to-execute-pegdbserver-console-exe/m-p/1887898#M36614</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can specify interface and port when you start pegdbserver_console for example like this:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;pegdbserver_console.exe -startserver -device=NXP_S32K3xx_S32K312 -interface=USBMULTILINK -port=PEMB7D193&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;More commands you can find with&amp;nbsp;pegdbserver_console.exe --help&amp;nbsp; command.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 12:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-specify-PEmicro-to-execute-pegdbserver-console-exe/m-p/1887898#M36614</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2024-06-14T12:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: How to specify PEmicro to execute pegdbserver_console.exe -startserver -device=NXP_S32K146F1M0M1</title>
      <link>https://community.nxp.com/t5/S32K/How-to-specify-PEmicro-to-execute-pegdbserver-console-exe/m-p/1939847#M40081</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to specify a PE to start a corresponding service when using the command line, but my specification doesn't seem to take effect; it keeps using the default value. As shown in the image, my computer is connected to two PEs: PE5748112 and PE5750673. However, when I try to specify PE5750673 using "-port" or "-PORT," it still defaults to using PE5748112, which is the HW Auto-Selected case. How can I resolve this issue?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Aug 2024 03:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-specify-PEmicro-to-execute-pegdbserver-console-exe/m-p/1939847#M40081</guid>
      <dc:creator>Jackey_cj</dc:creator>
      <dc:date>2024-08-26T03:01:51Z</dc:date>
    </item>
  </channel>
</rss>