<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344-Fee sample software in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1886291#M36510</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218611"&gt;@Simon-Liu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I apologize for the inconveniences, but those examples are currently the only ones available.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jun 2024 16:46:45 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-06-12T16:46:45Z</dc:date>
    <item>
      <title>S32K344-Fee sample software</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1884890#M36429</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I used the S32DS tool to generate the Fee sample software. I saw that the Fee, MemAcc and Mem_43_INFLS components were generated in the MCAL layer. And the fee interface was used in the main function to perform read and write operations.&lt;BR /&gt;But I noticed that it is inconvenient to use the Fee read and write interface to perform operations. After each read and write, the functions Fee_MainFunction() and MemAcc_MainFunction() need to be polled to perform the corresponding actions, which is not practical in actual applications.&lt;BR /&gt;Do you have an upper-level Flash data storage management module? Like the sample code of the NVM module in AutoSar?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 07:51:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1884890#M36429</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-06-11T07:51:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-Fee sample software</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1885381#M36457</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218611"&gt;@Simon-Liu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can look into the C40_Ip_Example_S32K344, which i&lt;SPAN&gt;nitializes IP C40 driver and erase, write, read internal flash memory.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 17:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1885381#M36457</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-06-11T17:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-Fee sample software</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1886101#M36497</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;But the software I mentioned before is not a simple software example for reading, writing and erasing Flash.&lt;BR /&gt;It is a software module that manages Fee Block on the upper layer of MemAcc and Fee, similar to the Nvm module in AutoSar.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 11:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1886101#M36497</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-06-12T11:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-Fee sample software</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1886291#M36510</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218611"&gt;@Simon-Liu&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I apologize for the inconveniences, but those examples are currently the only ones available.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 16:46:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Fee-sample-software/m-p/1886291#M36510</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-06-12T16:46:45Z</dc:date>
    </item>
  </channel>
</rss>