<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Program not starting after power on</title>
    <link>https://community.nxp.com/t5/S32K/Program-not-starting-after-power-on/m-p/1886011#M36493</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Kind of a stupid question, but I can seem to find why this doesn't work.&lt;/P&gt;&lt;P&gt;I am using a S32K144W. When debugging everything works fine and I can develop my application. However, when I disconnect the debugger (JLink) and power cycle my board, nothing happens. Pressing the reset button doesn't work. The application doesn't start.&lt;/P&gt;&lt;P&gt;When I attach my debugger and start the gdb server, the application does run when pressing the reset button.&lt;/P&gt;&lt;P&gt;Can you provide any pointer to why this is and how to solve this problem?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jun 2024 09:29:30 GMT</pubDate>
    <dc:creator>peacefulcarrot</dc:creator>
    <dc:date>2024-06-12T09:29:30Z</dc:date>
    <item>
      <title>Program not starting after power on</title>
      <link>https://community.nxp.com/t5/S32K/Program-not-starting-after-power-on/m-p/1886011#M36493</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Kind of a stupid question, but I can seem to find why this doesn't work.&lt;/P&gt;&lt;P&gt;I am using a S32K144W. When debugging everything works fine and I can develop my application. However, when I disconnect the debugger (JLink) and power cycle my board, nothing happens. Pressing the reset button doesn't work. The application doesn't start.&lt;/P&gt;&lt;P&gt;When I attach my debugger and start the gdb server, the application does run when pressing the reset button.&lt;/P&gt;&lt;P&gt;Can you provide any pointer to why this is and how to solve this problem?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 09:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-not-starting-after-power-on/m-p/1886011#M36493</guid>
      <dc:creator>peacefulcarrot</dc:creator>
      <dc:date>2024-06-12T09:29:30Z</dc:date>
    </item>
    <item>
      <title>Re: Program not starting after power on</title>
      <link>https://community.nxp.com/t5/S32K/Program-not-starting-after-power-on/m-p/1886591#M36532</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@peacefulcarrot" target="_blank"&gt;Hi@peacefulcarrot&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I have encountered some similar problems, and the reason for the failure was that the clock did not run&lt;/P&gt;
&lt;P&gt;properly.You can check if there is any problem with the clock configuration&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 05:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-not-starting-after-power-on/m-p/1886591#M36532</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-06-13T05:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: Program not starting after power on</title>
      <link>https://community.nxp.com/t5/S32K/Program-not-starting-after-power-on/m-p/1886746#M36544</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;After some more testing the issue seemed to be the fact that I went to VLPS power mode. No idea why it works when the debugging is connected.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 07:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-not-starting-after-power-on/m-p/1886746#M36544</guid>
      <dc:creator>peacefulcarrot</dc:creator>
      <dc:date>2024-06-13T07:57:22Z</dc:date>
    </item>
  </channel>
</rss>