<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic measure PWM frequency in S32K</title>
    <link>https://community.nxp.com/t5/S32K/measure-PWM-frequency/m-p/1881953#M36275</link>
    <description>&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Hello i am using s32k142, and i am generating pwm using ftm timer.&lt;BR /&gt;Is there a possibility to calculate the number of rising edges that we output from the pin, can this be done in some way, because i will keep increase the pwm frequency so i can’t do it using a timer, that’s why i would prefer if we can calculate the number of pin’s own pulses that are generated&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jun 2024 21:07:14 GMT</pubDate>
    <dc:creator>Othmane1</dc:creator>
    <dc:date>2024-06-05T21:07:14Z</dc:date>
    <item>
      <title>measure PWM frequency</title>
      <link>https://community.nxp.com/t5/S32K/measure-PWM-frequency/m-p/1881953#M36275</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Hello i am using s32k142, and i am generating pwm using ftm timer.&lt;BR /&gt;Is there a possibility to calculate the number of rising edges that we output from the pin, can this be done in some way, because i will keep increase the pwm frequency so i can’t do it using a timer, that’s why i would prefer if we can calculate the number of pin’s own pulses that are generated&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jun 2024 21:07:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/measure-PWM-frequency/m-p/1881953#M36275</guid>
      <dc:creator>Othmane1</dc:creator>
      <dc:date>2024-06-05T21:07:14Z</dc:date>
    </item>
    <item>
      <title>Re: measure PWM frequency</title>
      <link>https://community.nxp.com/t5/S32K/measure-PWM-frequency/m-p/1882174#M36280</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;Othmane1&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;You may need to connect the output PIN to some input pins of the MCU through external lines.&lt;BR /&gt;1. Implement it through the GPIO port input interrupt and a timer&lt;BR /&gt;2. Implement it through the FTM input capture module&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 01:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/measure-PWM-frequency/m-p/1882174#M36280</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-06-06T01:42:02Z</dc:date>
    </item>
  </channel>
</rss>