<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is TDC is really needed in CANFD in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Is-TDC-is-really-needed-in-CANFD/m-p/1879681#M36147</link>
    <description>&lt;P&gt;Yes got it,Thankyou&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jun 2024 09:05:06 GMT</pubDate>
    <dc:creator>deepika_16</dc:creator>
    <dc:date>2024-06-03T09:05:06Z</dc:date>
    <item>
      <title>Is TDC is really needed in CANFD</title>
      <link>https://community.nxp.com/t5/S32K/Is-TDC-is-really-needed-in-CANFD/m-p/1875350#M35818</link>
      <description>&lt;P&gt;&amp;nbsp;When enabling CANFD Is "&lt;STRONG&gt;Transceiver Delay Compensation&lt;/STRONG&gt;" is needs to enabled when it is in Data phase. If needed why we need to enable and also If not why it is not needed to enable TDC?&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 08:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-TDC-is-really-needed-in-CANFD/m-p/1875350#M35818</guid>
      <dc:creator>deepika_16</dc:creator>
      <dc:date>2024-05-27T08:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: Is TDC is really needed in CANFD</title>
      <link>https://community.nxp.com/t5/S32K/Is-TDC-is-really-needed-in-CANFD/m-p/1875517#M35832</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;TDC is not necessarily needed for lower rates (&amp;lt;3-4Mbits). But if enabled, must be properly set.&lt;BR /&gt;TDC is needed for higher rates when transceiver loop delay becomes bigger then CAN bit time so CAN module is not able to detect properly transmitted bits. So in order to compensate for this loop delay when checking for bit errors, a Secondary Sample-Point (SSP) is defined and instead at the Sample-Point, the transmitted bits are checked at the SSP.&lt;/P&gt;
&lt;P&gt;More description and the formula is given in chapter 72.3.10.3 Transceiver delay compensation of the S32K3 RM.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 11:03:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-TDC-is-really-needed-in-CANFD/m-p/1875517#M35832</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-05-27T11:03:45Z</dc:date>
    </item>
    <item>
      <title>Re: Is TDC is really needed in CANFD</title>
      <link>https://community.nxp.com/t5/S32K/Is-TDC-is-really-needed-in-CANFD/m-p/1879681#M36147</link>
      <description>&lt;P&gt;Yes got it,Thankyou&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jun 2024 09:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-TDC-is-really-needed-in-CANFD/m-p/1879681#M36147</guid>
      <dc:creator>deepika_16</dc:creator>
      <dc:date>2024-06-03T09:05:06Z</dc:date>
    </item>
  </channel>
</rss>