<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32k312 program in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-program/m-p/1878572#M36043</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am using S32K312EVB-Q172. The current PROJECT works normally in DEBUG mode.&lt;BR /&gt;My question is about burning. I used J-link to burn the bin file generated by the above project to the 0x400000 position. It showed that the burning was successful, but the program was not being executed.&lt;BR /&gt;I would like to ask if there are any steps or settings that are missing?&lt;/P&gt;</description>
    <pubDate>Fri, 31 May 2024 03:48:25 GMT</pubDate>
    <dc:creator>lua40927</dc:creator>
    <dc:date>2024-05-31T03:48:25Z</dc:date>
    <item>
      <title>s32k312 program</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-program/m-p/1878572#M36043</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I am using S32K312EVB-Q172. The current PROJECT works normally in DEBUG mode.&lt;BR /&gt;My question is about burning. I used J-link to burn the bin file generated by the above project to the 0x400000 position. It showed that the burning was successful, but the program was not being executed.&lt;BR /&gt;I would like to ask if there are any steps or settings that are missing?&lt;/P&gt;</description>
      <pubDate>Fri, 31 May 2024 03:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-program/m-p/1878572#M36043</guid>
      <dc:creator>lua40927</dc:creator>
      <dc:date>2024-05-31T03:48:25Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 program</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-program/m-p/1878845#M36083</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;This may caused by &lt;SPAN&gt;incorrect&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN&gt;ratio between&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;HSE_CLK&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;and&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;APIS_SLOW_CLK&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;set by the&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;Clocks Tool&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;in&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;S32CT&lt;/EM&gt;&lt;SPAN&gt;. For more detail, please read the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/If-I-don-t-give-s32k312-delay-the-CAN-stop-during-operation/m-p/1828163/highlight/false#M32968" target="_self"&gt;If I don't give s32k312 delay, the CAN stop during operation&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 31 May 2024 09:12:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-program/m-p/1878845#M36083</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-05-31T09:12:10Z</dc:date>
    </item>
  </channel>
</rss>