<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 Port Update Code in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-Port-Update-Code/m-p/1878055#M36020</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Maybe it is caused by installing multiple versions of S32K3 RTD in S32DS v3.4.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;&lt;SPAN class=" copy-paste-block"&gt;If you installed both RTD RTM 1.0.0 and RTM 2.0.0, to avoid&amp;nbsp;project RTD version auto conversion which would break up the&amp;nbsp;old version projects, try to remove the&amp;nbsp; “compatibility.xml”&amp;nbsp;&lt;BR /&gt;located at “C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration”"&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 30 May 2024 09:09:34 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-05-30T09:09:34Z</dc:date>
    <item>
      <title>S32K312 Port Update Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Port-Update-Code/m-p/1877708#M35984</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I get this error when generating after setting up a port, where should I fix it so it doesn't happen?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can fix it and use it, but I want to set it so that I don't get this error in the future.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I don't see any modifications in the component settings.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="coo_0-1717030961163.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/281614iA75B346D640F7DB1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="coo_0-1717030961163.png" alt="coo_0-1717030961163.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;coo_0-1717030961163.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 May 2024 01:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Port-Update-Code/m-p/1877708#M35984</guid>
      <dc:creator>coo</dc:creator>
      <dc:date>2024-05-30T01:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 Port Update Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Port-Update-Code/m-p/1878055#M36020</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Maybe it is caused by installing multiple versions of S32K3 RTD in S32DS v3.4.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider a b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;&lt;SPAN class=" copy-paste-block"&gt;If you installed both RTD RTM 1.0.0 and RTM 2.0.0, to avoid&amp;nbsp;project RTD version auto conversion which would break up the&amp;nbsp;old version projects, try to remove the&amp;nbsp; “compatibility.xml”&amp;nbsp;&lt;BR /&gt;located at “C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration”"&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 30 May 2024 09:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Port-Update-Code/m-p/1878055#M36020</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-05-30T09:09:34Z</dc:date>
    </item>
  </channel>
</rss>