<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Why PIT is needed in S32K?</title>
    <link>https://community.nxp.com/t5/S32K/Why-PIT-is-needed-in-S32K/m-p/1876551#M35910</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231277"&gt;@deepika_16&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;PIT decrements from set value to zero and STM increments from zero to set value.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Also, all the PIT instances are capable of generating periodic triggers. PIT triggers are routed to motor control IPs such as eMIOS, LCU, BCTU, ADC etc. via TRGMUX.&amp;nbsp;It also&amp;nbsp;&lt;SPAN&gt;contains RTI which can be used for waking up from STOP mode and PIT can be used to trigger DMA.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 28 May 2024 21:25:54 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-05-28T21:25:54Z</dc:date>
    <item>
      <title>Why PIT is needed in S32K?</title>
      <link>https://community.nxp.com/t5/S32K/Why-PIT-is-needed-in-S32K/m-p/1875929#M35856</link>
      <description>&lt;P&gt;Why PIT is needed for partition of clock gating even though we are having STM timers based on core clock frequency we are supplying the clock to STM?&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 05:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Why-PIT-is-needed-in-S32K/m-p/1875929#M35856</guid>
      <dc:creator>deepika_16</dc:creator>
      <dc:date>2024-05-28T05:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: Why PIT is needed in S32K?</title>
      <link>https://community.nxp.com/t5/S32K/Why-PIT-is-needed-in-S32K/m-p/1876551#M35910</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231277"&gt;@deepika_16&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;PIT decrements from set value to zero and STM increments from zero to set value.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Also, all the PIT instances are capable of generating periodic triggers. PIT triggers are routed to motor control IPs such as eMIOS, LCU, BCTU, ADC etc. via TRGMUX.&amp;nbsp;It also&amp;nbsp;&lt;SPAN&gt;contains RTI which can be used for waking up from STOP mode and PIT can be used to trigger DMA.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 21:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Why-PIT-is-needed-in-S32K/m-p/1876551#M35910</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-05-28T21:25:54Z</dc:date>
    </item>
  </channel>
</rss>