<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K314-RAM size issue</title>
    <link>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1876144#M35880</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I saw in Table 5.S32K3xx chip's feature comparison in the S323XXRM manual that the RAM of the S32K314 has 512KB, which contains 96KB of TCM.&lt;BR /&gt;But in Table 90.Memory configuration, S32K314 has 160KB SRAM0 and 160KB SRAM1, as well as 32kB ITCM and 64KB DTCM.&lt;BR /&gt;All the above mentioned RAMs total only 416KB, which is 96KB short of 512KB. Where is this 96KB?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
    <pubDate>Tue, 28 May 2024 08:39:27 GMT</pubDate>
    <dc:creator>Simon-Liu</dc:creator>
    <dc:date>2024-05-28T08:39:27Z</dc:date>
    <item>
      <title>S32K314-RAM size issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1876144#M35880</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I saw in Table 5.S32K3xx chip's feature comparison in the S323XXRM manual that the RAM of the S32K314 has 512KB, which contains 96KB of TCM.&lt;BR /&gt;But in Table 90.Memory configuration, S32K314 has 160KB SRAM0 and 160KB SRAM1, as well as 32kB ITCM and 64KB DTCM.&lt;BR /&gt;All the above mentioned RAMs total only 416KB, which is 96KB short of 512KB. Where is this 96KB?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 08:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1876144#M35880</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-05-28T08:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314-RAM size issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1876896#M35934</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;That is the TCM from other core. You can use it even if core is not present via backdoor access.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1716965588353.png" style="width: 700px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/281316i373F25D5E2BEC450/image-dimensions/700x581?v=v2" width="700" height="581" role="button" title="petervlna_0-1716965588353.png" alt="petervlna_0-1716965588353.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 May 2024 06:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1876896#M35934</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-05-29T06:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314-RAM size issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1876914#M35938</link>
      <description>&lt;P&gt;Hello Peter,&lt;/P&gt;&lt;P&gt;But according to the record in this table, S32K314 has only one core, how can I use the TCM of other cores?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SimonLiu_0-1716966772061.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/281322iC111C0E3022275C9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SimonLiu_0-1716966772061.png" alt="SimonLiu_0-1716966772061.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 May 2024 07:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1876914#M35938</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-05-29T07:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314-RAM size issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1877967#M36006</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes there is only one core. But you can use whole TCM.&lt;/P&gt;
&lt;P&gt;You will just access it via backdoor. You can see the address in the memory map for backdoor access are different as I have posted earlier.&lt;/P&gt;
&lt;P&gt;You will use backdoor for any other master except core which is tight to memory. For example also for DMA access.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 30 May 2024 07:18:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1877967#M36006</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-05-30T07:18:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314-RAM size issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1877977#M36009</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;That means other Masters including Core M7_0 can also access TCM1 through the backdoor, right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Thu, 30 May 2024 07:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1877977#M36009</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-05-30T07:25:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314-RAM size issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1878678#M36056</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;yes, that is the case.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 31 May 2024 06:36:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RAM-size-issue/m-p/1878678#M36056</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-05-31T06:36:13Z</dc:date>
    </item>
  </channel>
</rss>