<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックK142 LIN</title>
    <link>https://community.nxp.com/t5/S32K/K142-LIN/m-p/1874978#M35791</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I am using the K142EVB-Q100 development board and S32DS IDE. However, when I download the official demo and act as the master node, I can't capture the LIN frame header with an oscilloscope on the LIN line; there is only a continuous high level. When I measure the LIN TX pin directly, there is a signal, but it is still not the waveform of the frame header.I don't know why?(the photo is LIN-TX)&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Cache_-1c6c9325d565cf8d.jpg" style="width: 450px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/280834i580DB828EC0F377C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Cache_-1c6c9325d565cf8d.jpg" alt="Cache_-1c6c9325d565cf8d.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 25 May 2024 07:53:19 GMT</pubDate>
    <dc:creator>steve007</dc:creator>
    <dc:date>2024-05-25T07:53:19Z</dc:date>
    <item>
      <title>K142 LIN</title>
      <link>https://community.nxp.com/t5/S32K/K142-LIN/m-p/1874978#M35791</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am using the K142EVB-Q100 development board and S32DS IDE. However, when I download the official demo and act as the master node, I can't capture the LIN frame header with an oscilloscope on the LIN line; there is only a continuous high level. When I measure the LIN TX pin directly, there is a signal, but it is still not the waveform of the frame header.I don't know why?(the photo is LIN-TX)&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Cache_-1c6c9325d565cf8d.jpg" style="width: 450px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/280834i580DB828EC0F377C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Cache_-1c6c9325d565cf8d.jpg" alt="Cache_-1c6c9325d565cf8d.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 25 May 2024 07:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K142-LIN/m-p/1874978#M35791</guid>
      <dc:creator>steve007</dc:creator>
      <dc:date>2024-05-25T07:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: K142 LIN</title>
      <link>https://community.nxp.com/t5/S32K/K142-LIN/m-p/1875231#M35808</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;not sure of exact example you are referring to. Here it seems a LIN transceiver is not active, so be sure board is powered by 12V and transceiver's SLP pin is held high by MCU.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 06:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K142-LIN/m-p/1875231#M35808</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-05-27T06:15:58Z</dc:date>
    </item>
  </channel>
</rss>