<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Reflash Process</title>
    <link>https://community.nxp.com/t5/S32K/Reflash-Process/m-p/852415#M3569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Emmanuel Aguilasocho&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Device functionality is guaranteed up to the LVR assert level (2.7 V as Min.). So Inside the operating rating of the MCU, the device should operate correctly and the flash memory can be guaranteed.&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hope this helps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 02 Mar 2019 01:21:39 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-03-02T01:21:39Z</dc:date>
    <item>
      <title>Reflash Process</title>
      <link>https://community.nxp.com/t5/S32K/Reflash-Process/m-p/852414#M3568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before writing flash memory, is it recommended to verify the MCU source voltage to be into a minimal level?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 17:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Reflash-Process/m-p/852414#M3568</guid>
      <dc:creator>emmanuelaguilas</dc:creator>
      <dc:date>2019-02-26T17:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: Reflash Process</title>
      <link>https://community.nxp.com/t5/S32K/Reflash-Process/m-p/852415#M3569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Emmanuel Aguilasocho&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Device functionality is guaranteed up to the LVR assert level (2.7 V as Min.). So Inside the operating rating of the MCU, the device should operate correctly and the flash memory can be guaranteed.&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hope this helps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Mar 2019 01:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Reflash-Process/m-p/852415#M3569</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-03-02T01:21:39Z</dc:date>
    </item>
  </channel>
</rss>