<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TJA1153 PINOUT &amp;amp; Datasheet in S32K</title>
    <link>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867205#M35473</link>
    <description>Hi&lt;BR /&gt;When I checked Evaluation boards BOM, S32K312EVB is using TJA1043TKY part and S32K3X4EVB is using TJA1443ATK but in the interface list it is shown as TJA1153 is used in S32K3X4EVB.&lt;BR /&gt;&lt;BR /&gt;Can you please clarify this.</description>
    <pubDate>Thu, 16 May 2024 13:27:51 GMT</pubDate>
    <dc:creator>KarthikRaja</dc:creator>
    <dc:date>2024-05-16T13:27:51Z</dc:date>
    <item>
      <title>TJA1153 PINOUT &amp; Datasheet</title>
      <link>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867184#M35472</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For a product development, we are planning to use S32K MCU along with Secure CAN chip TJA1153. Could you provide technical datasheet as I could not find in online. I need to know the PINOUT, voltage levels, operating modes and other features.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Karthik Raja&lt;/P&gt;</description>
      <pubDate>Thu, 16 May 2024 12:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867184#M35472</guid>
      <dc:creator>KarthikRaja</dc:creator>
      <dc:date>2024-05-16T12:49:26Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153 PINOUT &amp; Datasheet</title>
      <link>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867205#M35473</link>
      <description>Hi&lt;BR /&gt;When I checked Evaluation boards BOM, S32K312EVB is using TJA1043TKY part and S32K3X4EVB is using TJA1443ATK but in the interface list it is shown as TJA1153 is used in S32K3X4EVB.&lt;BR /&gt;&lt;BR /&gt;Can you please clarify this.</description>
      <pubDate>Thu, 16 May 2024 13:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867205#M35473</guid>
      <dc:creator>KarthikRaja</dc:creator>
      <dc:date>2024-05-16T13:27:51Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153 PINOUT &amp; Datasheet</title>
      <link>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867214#M35474</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;And also when I checked S32K3X4EVB interfaces it is given as TJA1153 is used but when I checked BOM I found TJA1443ATK chip is used. But I see TJA1443 chip is not secure CAN.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you clarify this, or secure CAN is something to do with algorithms?&lt;/P&gt;</description>
      <pubDate>Thu, 16 May 2024 13:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867214#M35474</guid>
      <dc:creator>KarthikRaja</dc:creator>
      <dc:date>2024-05-16T13:30:10Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153 PINOUT &amp; Datasheet</title>
      <link>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867765#M35507</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Karthik,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The TJA1153A datasheet&amp;nbsp;as well as other useful documentation are classified as Secure Files requiring an NDA.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If your company has not signed the NDA with NXP yet, you can request it from:&lt;BR /&gt;&lt;A href="https://www.nxp.com/support/support:SUPPORTHOME" target="_blank" rel="noopener"&gt;https://www.nxp.com/support/support:SUPPORTHOME&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If there is a valid NDA in place, you can download the datasheet from:&lt;BR /&gt;&lt;A href="https://www.nxp.com/products/interfaces/can-transceivers/secure-can-transceivers/secure-hs-can-transceiver-with-sleep-mode:TJA1153" target="_blank" rel="noopener"&gt;https://www.nxp.com/products/interfaces/can-transceivers/secure-can-transceivers/secure-hs-can-transceiver-with-sleep-mode:TJA1153&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture 2.JPG" style="width: 593px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/279304iEE4F5A34CB637268/image-dimensions/593x558?v=v2" width="593" height="558" role="button" title="Capture 2.JPG" alt="Capture 2.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture 2.JPG&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please make sure you are signed in to&amp;nbsp;&lt;A href="https://nxp.com/" target="_blank"&gt;nxp.com&lt;/A&gt;. If you do not see the datasheet, please click on "Request additional access" or&amp;nbsp;edit your secure access rights by going to My NXP &amp;gt; Profile.&amp;nbsp;For more information about secure access rights, please refer to this website:&lt;BR /&gt;&lt;A href="https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS" target="_blank"&gt;https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;The TJA1153A is a standalone HS-CAN transceiver with Sleep mode offering these security features:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture 3.JPG" style="width: 553px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/279306iA3016993ACC50FB8/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture 3.JPG" alt="Capture 3.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture 3.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In case there are no security violations detected, the TJA1153A behaves like a standard HS-CAN transceiver such as the TJA1443ATK.&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 06:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1867765#M35507</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-05-17T06:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153 PINOUT &amp; Datasheet</title>
      <link>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1868798#M35571</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for that information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;When I checked Evaluation boards BOM, S32K3X4EVB is using TJA1443ATK but in the interface list &amp;amp; in the block diagram it is shown as TJA1153.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Are both same or why it is still given like this. Kindly clarify which CAN transceiver is used in&amp;nbsp;&lt;SPAN&gt;S32K3X4EVB board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 May 2024 10:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1153-PINOUT-amp-Datasheet/m-p/1868798#M35571</guid>
      <dc:creator>KarthikRaja</dc:creator>
      <dc:date>2024-05-20T10:04:27Z</dc:date>
    </item>
  </channel>
</rss>