<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K341 QuadSPI</title>
    <link>https://community.nxp.com/t5/S32K/S32K341-QuadSPI/m-p/1867156#M35468</link>
    <description>&lt;P&gt;Thank you for the answer. I am communicating with the device with through ARM DAP. I am relaying on the drivers but not using them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I managed to properly initialize the device. Now I want to read the ID of the Ext flash. I am sending proper command, and getting right answer. RBSR register shows that new data appeared in the buffer. But when I read the RDBR register there is no data in them.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 16 May 2024 12:09:46 GMT</pubDate>
    <dc:creator>Mateusz_K</dc:creator>
    <dc:date>2024-05-16T12:09:46Z</dc:date>
    <item>
      <title>S32K341 QuadSPI</title>
      <link>https://community.nxp.com/t5/S32K/S32K341-QuadSPI/m-p/1865456#M35343</link>
      <description>&lt;P&gt;I want to use external flash with S32K341. I am trying to read id of the external flash memory. When I try to do using IP command, I get stuck waiting for SR[BUSY] flag to become 0. Data, cs, and clk lines quiet. Data lines are in a high state, clk is low. I want to use internal FIRC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What steps duirng the initialization am i missing?&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. QuadSPI clock enable in&amp;nbsp;MC_ME&lt;/P&gt;&lt;P&gt;2. Pin setup, copied from the example in RTD package, considering S32K342 quad spi.&lt;/P&gt;&lt;P&gt;3. Enable QuadSPI by MCR module&lt;/P&gt;&lt;P&gt;4. Unlocking LUT, writing sequence (cmd(0x9F), read, stop) on 0 index, locking LUT&lt;/P&gt;&lt;P&gt;5. Starting by writing address 0x00 to SFAR and 0 to IPCR[SEQID], 4 to&amp;nbsp; IDATSZ&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why are the no signal on data lines?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 13:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K341-QuadSPI/m-p/1865456#M35343</guid>
      <dc:creator>Mateusz_K</dc:creator>
      <dc:date>2024-05-14T13:39:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K341 QuadSPI</title>
      <link>https://community.nxp.com/t5/S32K/S32K341-QuadSPI/m-p/1866312#M35413</link>
      <description>&lt;P&gt;Why you are not using NXP drivers?&lt;/P&gt;
&lt;P&gt;A driver is a part of RTD FLS drivers pack (real-time time flash driver, supporting internal flash as well as QuadSPI):&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/automotive-software-and-tools/real-time-drivers-rtd:AUTOMOTIVE-RTD" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/software/automotive-software-and-tools/real-time-drivers-rtd:AUTOMOTIVE-RTD&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Otherwise there is an appnote dealing with &lt;SPAN&gt;QuadSPI:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12193.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12193.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;QuadSPI is highly configurable module because it uses look-up tables for SPI commands what should theoretically allow user to adapt the code to any SPI memory.&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 13:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K341-QuadSPI/m-p/1866312#M35413</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-05-15T13:00:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32K341 QuadSPI</title>
      <link>https://community.nxp.com/t5/S32K/S32K341-QuadSPI/m-p/1867156#M35468</link>
      <description>&lt;P&gt;Thank you for the answer. I am communicating with the device with through ARM DAP. I am relaying on the drivers but not using them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I managed to properly initialize the device. Now I want to read the ID of the Ext flash. I am sending proper command, and getting right answer. RBSR register shows that new data appeared in the buffer. But when I read the RDBR register there is no data in them.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 May 2024 12:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K341-QuadSPI/m-p/1867156#M35468</guid>
      <dc:creator>Mateusz_K</dc:creator>
      <dc:date>2024-05-16T12:09:46Z</dc:date>
    </item>
  </channel>
</rss>