<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: s32k312 Writing dflash Indicates whether the pflash program interrupts running</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1866637#M35430</link>
    <description>&lt;P&gt;hi, I used RTD 1.0.0.&amp;nbsp; And this question has been solved.&amp;nbsp;&lt;SPAN&gt;The solution can be found in the following link.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K/During-the-process-of-writing-dflash-if-an-interrupt-occurs-will/m-p/1866055/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExXN0lRVzlGRkJaSlowfDE4NjYwNTV8U1VCU0NSSVBUSU9OU3xoSw#M35386" target="_blank"&gt;https://community.nxp.com/t5/S32K/During-the-process-of-writing-dflash-if-an-interrupt-occurs-will/m-p/1866055/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExXN0lRVzlGRkJaSlowfDE4NjYwNTV8U1VCU0NSSVBUSU9OU3xoSw#M35386&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 16 May 2024 00:28:56 GMT</pubDate>
    <dc:creator>WenWenDar</dc:creator>
    <dc:date>2024-05-16T00:28:56Z</dc:date>
    <item>
      <title>s32k312 Writing dflash Indicates whether the pflash program interrupts running</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1864004#M35255</link>
      <description>&lt;P&gt;When I use S32K312 chip pflash storage program, dflash as storage data, that when I run the program, including a 10us interrupt program, then I write data to dflash in the main loop will affect the interrupt response? What if it does? Do you need to map interrupts to ram?&lt;BR /&gt;Looking forward to hearing from you. Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 04:23:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1864004#M35255</guid>
      <dc:creator>Neo1096</dc:creator>
      <dc:date>2024-05-13T04:23:43Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 Writing dflash Indicates whether the pflash program interrupts running</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1865090#M35312</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229677"&gt;@Neo1096&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;DFlash and PFlash are two separate blocks.&lt;/P&gt;
&lt;P&gt;The program can run from PFlash, which can include the vector table and ISRs, while the DFlash is being programmed.&lt;/P&gt;
&lt;P&gt;The ISRs must not access data in DFlash though.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 07:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1865090#M35312</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-05-14T07:33:38Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 Writing dflash Indicates whether the pflash program interrupts running</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1865141#M35317</link>
      <description>&lt;P&gt;hi, &lt;SPAN&gt;I enable an interrupt of 100us per cycle. Then I erase one sector of data flash.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I called an API function called "C40_Ip_MainInterfaceSectorErase"&amp;nbsp; to erase data flash&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;During erasure, interrupts cannot be responded to.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;After erasure,&amp;nbsp;interrupts can be responded to normally.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So,&amp;nbsp;how to achieve the goal to enter interrupts while erasing data flash?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Looking forward to your reply&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 08:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1865141#M35317</guid>
      <dc:creator>WenWenDar</dc:creator>
      <dc:date>2024-05-14T08:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 Writing dflash Indicates whether the pflash program interrupts running</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1866216#M35405</link>
      <description>&lt;P&gt;What version of the RTD drivers do you use?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 10:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1866216#M35405</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-05-15T10:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 Writing dflash Indicates whether the pflash program interrupts running</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1866637#M35430</link>
      <description>&lt;P&gt;hi, I used RTD 1.0.0.&amp;nbsp; And this question has been solved.&amp;nbsp;&lt;SPAN&gt;The solution can be found in the following link.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K/During-the-process-of-writing-dflash-if-an-interrupt-occurs-will/m-p/1866055/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExXN0lRVzlGRkJaSlowfDE4NjYwNTV8U1VCU0NSSVBUSU9OU3xoSw#M35386" target="_blank"&gt;https://community.nxp.com/t5/S32K/During-the-process-of-writing-dflash-if-an-interrupt-occurs-will/m-p/1866055/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExXN0lRVzlGRkJaSlowfDE4NjYwNTV8U1VCU0NSSVBUSU9OU3xoSw#M35386&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 May 2024 00:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-Writing-dflash-Indicates-whether-the-pflash-program/m-p/1866637#M35430</guid>
      <dc:creator>WenWenDar</dc:creator>
      <dc:date>2024-05-16T00:28:56Z</dc:date>
    </item>
  </channel>
</rss>