<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 GPIO DC electrical specifications in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1866516#M35422</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207529"&gt;@Chinnan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You could set your desired voltage input as a reference by configuring an ADC and using that value as a low or high.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Wed, 15 May 2024 18:36:20 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-05-15T18:36:20Z</dc:date>
    <item>
      <title>S32K3 GPIO DC electrical specifications</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865287#M35328</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;When i applied an varying voltage from 0 to 3.3V to controller Pin, The microcontroller taking 1.65 as Input high. Also when i decrease high to low (Ie, 3.3V to 0V) at 1.58V microcontroller took as Input Low.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;As per data sheet, For 3.3V microcontroller Input high voltage is 0.7 VDD to VDD and Input low is 0V to 0.3 VDD.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;1, Why microcontroller taking 1.65 as Input high? Any software setting required to change or not?&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;2, What will actually happen in between an voltage comes VIL and VIH?&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;&lt;FONT&gt;3, What is the transition voltage of microcontroller?&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 09:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865287#M35328</guid>
      <dc:creator>Chinnan</dc:creator>
      <dc:date>2024-05-14T09:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 GPIO DC electrical specifications</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865291#M35329</link>
      <description>&lt;P&gt;The Microcontroller was &lt;SPAN&gt;S32K322NHT0MPAST&lt;/SPAN&gt; &amp;nbsp;100 Pin HDQFP&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 09:49:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865291#M35329</guid>
      <dc:creator>Chinnan</dc:creator>
      <dc:date>2024-05-14T09:49:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 GPIO DC electrical specifications</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865607#M35351</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207529"&gt;@Chinnan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can find inside the following document, section "Input Characteristics":&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2434.pdf?_gl=1*1p52xg5*_ga*MTg0ODMxMTEzMC4xNzE1NzA0MTgx*_ga_WM5LE0KMSH*MTcxNTcwNTg2MS4xLjEuMTcxNTcwNzQ2Ni4wLjAuMA.." target="_blank"&gt;AN2434: Input/Output Pin Drivers on HCS12 Family MCUs&lt;/A&gt;, which still applies to S32K3 family:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1715708563505.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/278737iC0F503EAF6EB9F44/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1715708563505.png" alt="Julin_AragnM_0-1715708563505.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_0-1715708563505.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;When defining VIH or VIL, it is generally set at 70% or 30% of VDD so &lt;SPAN&gt;it is guaranteed that the input reads&lt;/SPAN&gt;&amp;nbsp;either LOW or HIGH when input passes those thresholds levels.&lt;/P&gt;
&lt;P&gt;Many factors affect the transition voltage level for the MCU, such as temperature. That is why a specific transition voltage is not specified, it is not possible to predict which logic level the MCU will interpret.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 17:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865607#M35351</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-05-14T17:48:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 GPIO DC electrical specifications</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865983#M35380</link>
      <description>&lt;P&gt;Is there any way in the software that any input voltage between 0.3VDD to 0.65VDD on the GPIO pin can be taken as low or high?&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 06:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1865983#M35380</guid>
      <dc:creator>Chinnan</dc:creator>
      <dc:date>2024-05-15T06:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 GPIO DC electrical specifications</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1866516#M35422</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207529"&gt;@Chinnan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You could set your desired voltage input as a reference by configuring an ADC and using that value as a low or high.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 18:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-GPIO-DC-electrical-specifications/m-p/1866516#M35422</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-05-15T18:36:20Z</dc:date>
    </item>
  </channel>
</rss>