<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: LPSPI SEND question.</title>
    <link>https://community.nxp.com/t5/S32K/LPSPI-SEND-question/m-p/1865865#M35373</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As the Master, you should at least initialize the Serial Clock pin.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 15 May 2024 03:27:19 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-05-15T03:27:19Z</dc:date>
    <item>
      <title>LPSPI SEND question.</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-SEND-question/m-p/1864911#M35308</link>
      <description>&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;hi.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;i would like to use the send function of LPSPI0.&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;(LPSPI_DRV_MasterTransferBlocking)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;but now there is no signal.(oscilloscope)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attachment 1. H/W circuit diagram.&lt;/P&gt;&lt;P&gt;Attachment 2. config setting.&lt;/P&gt;&lt;P&gt;Attachment 3. code init.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have a question here.&lt;/P&gt;&lt;P&gt;Is transmisson possible even with only LPSPI0_OUT?&lt;/P&gt;&lt;P&gt;Or should I connect another pin? (ex. LPSPI0_PCS1)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;only the send function is needed.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;&lt;FONT&gt;what are the requirements for that feature?&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(i using 32K146)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 03:55:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-SEND-question/m-p/1864911#M35308</guid>
      <dc:creator>mswd</dc:creator>
      <dc:date>2024-05-14T03:55:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPSPI SEND question.</title>
      <link>https://community.nxp.com/t5/S32K/LPSPI-SEND-question/m-p/1865865#M35373</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As the Master, you should at least initialize the Serial Clock pin.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 03:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPSPI-SEND-question/m-p/1865865#M35373</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-05-15T03:27:19Z</dc:date>
    </item>
  </channel>
</rss>