<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Changing SPI framesize on S32K1 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Changing-SPI-framesize-on-S32K1/m-p/1865560#M35348</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;With 12bit (0-11) of Frame size of TCR register, what values we can set for the 12bit&amp;nbsp;of Frame size ?&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 14 May 2024 16:47:08 GMT</pubDate>
    <dc:creator>AnhNguyenDuc</dc:creator>
    <dc:date>2024-05-14T16:47:08Z</dc:date>
    <item>
      <title>Changing SPI framesize on S32K1</title>
      <link>https://community.nxp.com/t5/S32K/Changing-SPI-framesize-on-S32K1/m-p/1592457#M20400</link>
      <description>&lt;P&gt;Hello all,&lt;BR /&gt;I have a problem with the S32K146 and the SPI communication. But maybe the problem is due to my lack of knowledge about SPI communication. I have a device running as SPI master with framesize configured to 8 bits.&lt;BR /&gt;This setup works as expected. There are always 4 bytes exchanged between master and slave. So I want to change the framesize 8 to framesize 32.&lt;BR /&gt;However, then the received data is no longer valid. Do I have to consider other parameters when changing the framesize?&lt;BR /&gt;According to my theoretical understanding this should not be the case. However, maybe I am wrong....&lt;BR /&gt;I'm using the RTD driver V1.01.&lt;BR /&gt;Thank you for your help.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 15:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Changing-SPI-framesize-on-S32K1/m-p/1592457#M20400</guid>
      <dc:creator>superbird</dc:creator>
      <dc:date>2023-02-02T15:42:55Z</dc:date>
    </item>
    <item>
      <title>Re: Changing SPI framesize on S32K1</title>
      <link>https://community.nxp.com/t5/S32K/Changing-SPI-framesize-on-S32K1/m-p/1592694#M20403</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209845"&gt;@superbird&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The minimum frame size is 8 bits&lt;/LI&gt;
&lt;LI&gt;The minimum word size is 2 bits; a frame size of 33 bits (or similar) is not supported.&lt;/LI&gt;
&lt;LI&gt;If the frame size is larger than 32 bits, then the frame is divided into multiple words of 32-bits; each word is loaded from the transmit FIFO and stored in the receive FIFO separately.&lt;/LI&gt;
&lt;LI&gt;If the size of the frame is not divisible by 32, then the last load of the transmit FIFO and store of the receive FIFO will contain the remainder bits. For example, a 72-bit transfer will consist of 3 words:&lt;BR /&gt;the 1st and 2nd words are 32 bits, and the 3rd word is 8 bits.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;At RTD&amp;nbsp;Lpspi_Ip_UpdateFrameSize updates the frame size of the specific external device configuration for the following transfers.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 01:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Changing-SPI-framesize-on-S32K1/m-p/1592694#M20403</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-02-03T01:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: Changing SPI framesize on S32K1</title>
      <link>https://community.nxp.com/t5/S32K/Changing-SPI-framesize-on-S32K1/m-p/1865560#M35348</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;With 12bit (0-11) of Frame size of TCR register, what values we can set for the 12bit&amp;nbsp;of Frame size ?&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 16:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Changing-SPI-framesize-on-S32K1/m-p/1865560#M35348</guid>
      <dc:creator>AnhNguyenDuc</dc:creator>
      <dc:date>2024-05-14T16:47:08Z</dc:date>
    </item>
  </channel>
</rss>