<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 without  jlink or reset the program stop runing in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-without-jlink-or-reset-the-program-stop-runing/m-p/1865012#M35310</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/If-I-don-t-give-s32k312-delay-the-CAN-stop-during-operation/m-p/1828163/highlight/false#M32968" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;If I don't give s32k312 delay, the CAN stop during operation&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 14 May 2024 06:33:11 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-05-14T06:33:11Z</dc:date>
    <item>
      <title>S32K312 without  jlink or reset the program stop runing</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-without-jlink-or-reset-the-program-stop-runing/m-p/1863340#M35209</link>
      <description>&lt;P&gt;When I used S32DS to create the S32K312 project, the first time I burned the program, it ran normally, but when I tried to power on or reset it, the program stopped running.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="binZhang01_0-1715332566640.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/278181iAE590CF2BB13B310/image-size/medium?v=v2&amp;amp;px=400" role="button" title="binZhang01_0-1715332566640.png" alt="binZhang01_0-1715332566640.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;binZhang01_0-1715332566640.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32K3" id="S32K3"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#S32DS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 May 2024 09:31:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-without-jlink-or-reset-the-program-stop-runing/m-p/1863340#M35209</guid>
      <dc:creator>binZhang01</dc:creator>
      <dc:date>2024-05-10T09:31:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 without  jlink or reset the program stop runing</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-without-jlink-or-reset-the-program-stop-runing/m-p/1865012#M35310</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/If-I-don-t-give-s32k312-delay-the-CAN-stop-during-operation/m-p/1828163/highlight/false#M32968" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;If I don't give s32k312 delay, the CAN stop during operation&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 06:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-without-jlink-or-reset-the-program-stop-runing/m-p/1865012#M35310</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-05-14T06:33:11Z</dc:date>
    </item>
  </channel>
</rss>