<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Problem in FlexCAN1 transmit in S32K344</title>
    <link>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1864658#M35288</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232511"&gt;@sagar991&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you testing this with two S32K344 boards?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In order to see the signals for the transmissions, you will need another CAN node in the bus (either another MCU or CAN analyzer).&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián.&lt;/P&gt;</description>
    <pubDate>Mon, 13 May 2024 17:43:32 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-05-13T17:43:32Z</dc:date>
    <item>
      <title>Problem in FlexCAN1 transmit in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1862492#M35162</link>
      <description>&lt;P&gt;I enabled the pins configuration tool in the default FlexCAN_Ip_Example_S32K344 to observe the CAN0 Tx output on the PTA7 pin in the normal mode. I was able to see the digital CAN signals on the oscilloscope.&lt;BR /&gt;&lt;BR /&gt;But when I changed the output port from PTA7 to PTB1,&amp;nbsp;&lt;SPAN&gt;I couldn't see any signals on the oscilloscope&lt;/SPAN&gt;.&lt;BR /&gt;&lt;BR /&gt;I also tried changing CAN0 to CAN1, but still I can only see signals from the PTA7 port.&lt;BR /&gt;&lt;BR /&gt;Is there any reason why can't I observe CAN signals from any ports other than PTA7 becuase in schematics both PTA7 and PTB1 can have CAN0_Tx signal.&lt;BR /&gt;&lt;BR /&gt;I am using&amp;nbsp;S32K3X4EVB-T172 board have attached the project.&lt;/P&gt;</description>
      <pubDate>Thu, 09 May 2024 11:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1862492#M35162</guid>
      <dc:creator>sagar991</dc:creator>
      <dc:date>2024-05-09T11:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in FlexCAN1 transmit in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1864658#M35288</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232511"&gt;@sagar991&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you testing this with two S32K344 boards?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In order to see the signals for the transmissions, you will need another CAN node in the bus (either another MCU or CAN analyzer).&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián.&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 17:43:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1864658#M35288</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-05-13T17:43:32Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in FlexCAN1 transmit in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1867677#M35501</link>
      <description>&lt;P&gt;I have PCAN-USB CAN decoder which receives messages normally when CAN0 Tx pin is PTA7, but when I change it to PTB1, I don't receive any messages. Can only 1 pin be used in CAN0 for transmitting ?&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 05:08:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1867677#M35501</guid>
      <dc:creator>sagar991</dc:creator>
      <dc:date>2024-05-17T05:08:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in FlexCAN1 transmit in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1868301#M35533</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232511"&gt;@sagar991&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Sorry for the misunderstanding, only pins PTA6 &amp;amp; PTA7 are connected to the PHY on board:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1715982506795.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/279465iA60BDBE7F82209CB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1715982506795.png" alt="Julin_AragnM_0-1715982506795.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you need to use another pin for transmission, they need to be rerouted.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 21:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-FlexCAN1-transmit-in-S32K344/m-p/1868301#M35533</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-05-17T21:49:34Z</dc:date>
    </item>
  </channel>
</rss>