<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K344: eMIOS triggering the BCTU</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-triggering-the-BCTU/m-p/1864143#M35268</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I need the eMIOS to trigger the BCTU without interrupting the CPU. Currently, I am using the eMIOS GPT driver but I realized that if I remove the interrupt of eMIOS then triggering the BCTU stops.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Is it possible to trigger the BCTU via the eMIOS without CPU intervention?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 13 May 2024 07:27:19 GMT</pubDate>
    <dc:creator>Samuel_DCosta</dc:creator>
    <dc:date>2024-05-13T07:27:19Z</dc:date>
    <item>
      <title>S32K344: eMIOS triggering the BCTU</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-triggering-the-BCTU/m-p/1864143#M35268</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I need the eMIOS to trigger the BCTU without interrupting the CPU. Currently, I am using the eMIOS GPT driver but I realized that if I remove the interrupt of eMIOS then triggering the BCTU stops.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Is it possible to trigger the BCTU via the eMIOS without CPU intervention?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 07:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-eMIOS-triggering-the-BCTU/m-p/1864143#M35268</guid>
      <dc:creator>Samuel_DCosta</dc:creator>
      <dc:date>2024-05-13T07:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344: eMIOS triggering the BCTU</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-triggering-the-BCTU/m-p/1867519#M35490</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Yes! It is possible to trigger the BCTU via the eMIOS without CPU intervention, you can refer to the 4.2.4. Analogue data capturing from app note &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13767" target="_blank" rel="noopener"&gt;AN13767&lt;/A&gt;. Also you can check the config in its respective software in&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-motor-control-solutions/s32k344-brushless-direct-current-and-permanent-magnet-synchronous-motor-control-development-kit:MCSPTE1AK344" target="_blank" rel="noopener"&gt;MCSPTE1AK344&lt;/A&gt; page.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Thu, 16 May 2024 23:15:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-eMIOS-triggering-the-BCTU/m-p/1867519#M35490</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-05-16T23:15:42Z</dc:date>
    </item>
  </channel>
</rss>