<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックPhase shift FTM modules</title>
    <link>https://community.nxp.com/t5/S32K/Phase-shift-FTM-modules/m-p/635643#M351</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Goodmorning, can someone suggest me how can i realize a variable phase shift pwm using three FTM modules?&lt;/P&gt;&lt;P&gt;Need i to use some peripherals like PDB modules?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jan 2017 14:48:37 GMT</pubDate>
    <dc:creator>pietroserao</dc:creator>
    <dc:date>2017-01-20T14:48:37Z</dc:date>
    <item>
      <title>Phase shift FTM modules</title>
      <link>https://community.nxp.com/t5/S32K/Phase-shift-FTM-modules/m-p/635643#M351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Goodmorning, can someone suggest me how can i realize a variable phase shift pwm using three FTM modules?&lt;/P&gt;&lt;P&gt;Need i to use some peripherals like PDB modules?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 14:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Phase-shift-FTM-modules/m-p/635643#M351</guid>
      <dc:creator>pietroserao</dc:creator>
      <dc:date>2017-01-20T14:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: Phase shift FTM modules</title>
      <link>https://community.nxp.com/t5/S32K/Phase-shift-FTM-modules/m-p/635644#M352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the FTM module itself you can generate phase shift PWMs using Modified Combine PWM mode. This way up to 4 phase shift PWMs can be generated on single FTM module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12220i2FDD4A9D7E10F65F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you want to have FTM module counters somehow synchronized, the counter synchronization can be use and external HW trigger determines the time the FTM counter is reset.&lt;/P&gt;&lt;P&gt;The hardware trigger source can be from many other modules via TRGMUX, also FTM’s init and/or ext trigger can be used as HW trigger for FTM modules.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12197i3984CE0880EB5D5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2017 10:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Phase-shift-FTM-modules/m-p/635644#M352</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-01-23T10:37:01Z</dc:date>
    </item>
    <item>
      <title>Re: Phase shift FTM modules</title>
      <link>https://community.nxp.com/t5/S32K/Phase-shift-FTM-modules/m-p/635645#M353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you. Now i need to set the FTM0 and the FTM1 in the seguent operation mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When FTM counter is equal to a set treshold value then i will generate an external interrupt.&lt;BR /&gt;The FTM0 external interrupt is connected to the FTM1 HW1trigger by trigmux.&lt;/P&gt;&lt;P&gt;When the FTM1 HW1trigger is set, the ftm1 will generate a new pwm signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i generate an FTM0 external interrupt?&lt;/P&gt;&lt;P&gt;How can i reset the FTM1 pwm signal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 11:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Phase-shift-FTM-modules/m-p/635645#M353</guid>
      <dc:creator>pietroserao</dc:creator>
      <dc:date>2017-01-24T11:32:43Z</dc:date>
    </item>
  </channel>
</rss>