<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Writing data from UART with DMA in a new Array in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Writing-data-from-UART-with-DMA-in-a-new-Array/m-p/1858304#M34887</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I receive the data, but the problem is, that the CITER value from the ELINKNO register doesn't match with the value I got, when I write the registervalue in a variable.&lt;BR /&gt;Additionally the data in the recv_buf is not written from zero or the same field than in Msg.&lt;BR /&gt;I attached the DMA init and the code for the UART IRQ handler.&lt;/P&gt;&lt;P&gt;Please help me.&lt;/P&gt;&lt;P&gt;Sandra&lt;/P&gt;</description>
    <pubDate>Thu, 02 May 2024 08:12:31 GMT</pubDate>
    <dc:creator>12914A</dc:creator>
    <dc:date>2024-05-02T08:12:31Z</dc:date>
    <item>
      <title>Writing data from UART with DMA in a new Array</title>
      <link>https://community.nxp.com/t5/S32K/Writing-data-from-UART-with-DMA-in-a-new-Array/m-p/1858304#M34887</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I receive the data, but the problem is, that the CITER value from the ELINKNO register doesn't match with the value I got, when I write the registervalue in a variable.&lt;BR /&gt;Additionally the data in the recv_buf is not written from zero or the same field than in Msg.&lt;BR /&gt;I attached the DMA init and the code for the UART IRQ handler.&lt;/P&gt;&lt;P&gt;Please help me.&lt;/P&gt;&lt;P&gt;Sandra&lt;/P&gt;</description>
      <pubDate>Thu, 02 May 2024 08:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Writing-data-from-UART-with-DMA-in-a-new-Array/m-p/1858304#M34887</guid>
      <dc:creator>12914A</dc:creator>
      <dc:date>2024-05-02T08:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: Writing data from UART with DMA in a new Array</title>
      <link>https://community.nxp.com/t5/S32K/Writing-data-from-UART-with-DMA-in-a-new-Array/m-p/1859938#M35008</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232799"&gt;@12914A&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Have you read the register's value by debugging?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1715026234807.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/277297iE211C36CA3084869/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1715026234807.png" alt="Julin_AragnM_0-1715026234807.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_0-1715026234807.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can also test the example included with the example projects, which is based on the code in&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5413.pdf" target="_blank"&gt;AN5413: S32K1xx Series Cookbook.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_1-1715026240510.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/277298i9B59836ABE8C7F8E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_1-1715026240510.png" alt="Julin_AragnM_1-1715026240510.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_1-1715026240510.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 06 May 2024 20:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Writing-data-from-UART-with-DMA-in-a-new-Array/m-p/1859938#M35008</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-05-06T20:11:53Z</dc:date>
    </item>
  </channel>
</rss>