<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: NMI Handler (Non Maskable Interrupt) not triggering in S32K388</title>
    <link>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1855840#M34714</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;Can someone from NXP check this please?&lt;/P&gt;</description>
    <pubDate>Fri, 26 Apr 2024 16:28:19 GMT</pubDate>
    <dc:creator>punithchandra</dc:creator>
    <dc:date>2024-04-26T16:28:19Z</dc:date>
    <item>
      <title>NMI Handler (Non Maskable Interrupt) not triggering in S32K388</title>
      <link>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1851530#M34493</link>
      <description>&lt;P&gt;Hi Team,&lt;BR /&gt;&lt;BR /&gt;We are using the S32K388 eval board. We want to trigger the non-maskable interrupt when the pin PTD3 value changes.&lt;/P&gt;&lt;P&gt;We have configured PTD3 pin mode as SYSTEM_NMI_B. The pin PTD24 is configured as the GPIO output mode. We have connected the PTD3 &amp;amp; PTD24 via a wire on the IO matrix of the Eval board.&lt;/P&gt;&lt;P&gt;The code is written to toggle the PTD24 pin. Since this pin is connected to PTD3 which is configured as SYSTEM_NMI_B, we were expecting the breakpoint kept inside the NMI_Handler function to hit. But the breakpoint is never hit.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="punithchandra_0-1713778864226.png" style="width: 521px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274993iDC310217092E9BAC/image-dimensions/521x528?v=v2" width="521" height="528" role="button" title="punithchandra_0-1713778864226.png" alt="punithchandra_0-1713778864226.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="punithchandra_1-1713778975963.png" style="width: 553px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274994iF737F12301569FB7/image-dimensions/553x184?v=v2" width="553" height="184" role="button" title="punithchandra_1-1713778975963.png" alt="punithchandra_1-1713778975963.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We also have enabled this interrupt using the API&amp;nbsp;&lt;STRONG&gt;NVIC_EnableIRQ(NonMaskableInt_IRQn).&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;We are using the example code of Icu driver and did the changes as per our requirement.&lt;/P&gt;&lt;P&gt;Is there any other configuration parameter/ any code changes we need to do in order to enable this NMI interrupt?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32K3" id="S32K3"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;#NMI #Interrupt #ICU&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 09:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1851530#M34493</guid>
      <dc:creator>punithchandra</dc:creator>
      <dc:date>2024-04-22T09:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: NMI Handler (Non Maskable Interrupt) not triggering in S32K388</title>
      <link>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1852534#M34548</link>
      <description>&lt;P&gt;Hi Team,&lt;BR /&gt;&lt;BR /&gt;Can you please look into this query?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 13:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1852534#M34548</guid>
      <dc:creator>punithchandra</dc:creator>
      <dc:date>2024-04-23T13:09:33Z</dc:date>
    </item>
    <item>
      <title>Re: NMI Handler (Non Maskable Interrupt) not triggering in S32K388</title>
      <link>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1855840#M34714</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;Can someone from NXP check this please?&lt;/P&gt;</description>
      <pubDate>Fri, 26 Apr 2024 16:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1855840#M34714</guid>
      <dc:creator>punithchandra</dc:creator>
      <dc:date>2024-04-26T16:28:19Z</dc:date>
    </item>
    <item>
      <title>Re: NMI Handler (Non Maskable Interrupt) not triggering in S32K388</title>
      <link>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1886693#M36538</link>
      <description>&lt;P&gt;Configured the WakeupNMI configurations in the Icu module. And referred this in one of the IcuChannels. After this the NMI handler is being triggered.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="punithchandra_0-1718262939511.png" style="width: 669px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283895i7A4922FA38E91EB4/image-dimensions/669x273?v=v2" width="669" height="273" role="button" title="punithchandra_0-1718262939511.png" alt="punithchandra_0-1718262939511.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 07:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/NMI-Handler-Non-Maskable-Interrupt-not-triggering-in-S32K388/m-p/1886693#M36538</guid>
      <dc:creator>punithchandra</dc:creator>
      <dc:date>2024-06-13T07:16:01Z</dc:date>
    </item>
  </channel>
</rss>