<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CCP/XCP Protocol in S32K144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1855172#M34686</link>
    <description>&lt;P&gt;&lt;A href="mailto:Hi@prasannak9488" target="_blank"&gt;Hi@prasannak9488&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;As far as I know, we have no such example for customers to refer to.&lt;/P&gt;
&lt;P&gt;Usually CCP or XCP is provided by a third party, and most of them are paid.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Apr 2024 00:57:22 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2024-04-26T00:57:22Z</dc:date>
    <item>
      <title>CCP/XCP Protocol in S32K144</title>
      <link>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1853918#M34613</link>
      <description>&lt;P&gt;I am trying to use CCP/XCP protocol in my system to calibrate the ECU during the runtime ,I am not sure about whether S32K144 support the protocol,could some one help me clarify the doubt&lt;BR /&gt;Thank You.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 21:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1853918#M34613</guid>
      <dc:creator>prasannak9488</dc:creator>
      <dc:date>2024-04-24T21:01:47Z</dc:date>
    </item>
    <item>
      <title>Re: CCP/XCP Protocol in S32K144</title>
      <link>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1854285#M34625</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@prasannak9488" target="_blank"&gt;Hi@prasannak9488&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;below info comes from S32K1-RM&lt;/P&gt;
&lt;P&gt;55.2 Overview&lt;BR /&gt;The FlexCAN module is a communication controller implementing the CAN protocol&lt;BR /&gt;according to the ISO 11898-1 standard and CAN 2.0 B protocol specifications.&lt;BR /&gt;The CAN protocol was primarily designed to be used as a vehicle serial data bus, meeting&lt;BR /&gt;the specific real-time processing and reliable operation requirements in the EMI&lt;BR /&gt;environment of a vehicle. The FlexCAN module is a full implementation of the CAN&lt;BR /&gt;protocol specification, the CAN with Flexible Data rate (CAN FD) protocol, and the&lt;BR /&gt;CAN 2.0 version B protocol, which supports both standard and extended message frames&lt;BR /&gt;and long payloads.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.kvaser.com/about-can/higher-layer-protocols/ccpxcp/" target="_blank"&gt;https://www.kvaser.com/about-can/higher-layer-protocols/ccpxcp/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;CCP is &lt;STRONG&gt;a&lt;/STRONG&gt; &lt;STRONG&gt;application layer for CAN 2.0B&lt;/STRONG&gt; (11- or 29-bits CAN id). The Protocol is a top layer (layer 7) according to the OSI model, which means that the protocol does not describe how bits and bytes are created but uses the CAN 2.0B protocol physical, data link and network layer.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;You can see the S32K144's Flexcan module can support CAN 2.0 B, which can be support you to integrate CCP or XCP protocol.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 04:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1854285#M34625</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-04-25T04:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: CCP/XCP Protocol in S32K144</title>
      <link>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1854962#M34675</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;for the response. Is there any example that would help in implementing CCP in the system using model based application(Simulink)&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 17:00:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1854962#M34675</guid>
      <dc:creator>prasannak9488</dc:creator>
      <dc:date>2024-04-25T17:00:10Z</dc:date>
    </item>
    <item>
      <title>Re: CCP/XCP Protocol in S32K144</title>
      <link>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1855172#M34686</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@prasannak9488" target="_blank"&gt;Hi@prasannak9488&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;As far as I know, we have no such example for customers to refer to.&lt;/P&gt;
&lt;P&gt;Usually CCP or XCP is provided by a third party, and most of them are paid.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Apr 2024 00:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CCP-XCP-Protocol-in-S32K144/m-p/1855172#M34686</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-04-26T00:57:22Z</dc:date>
    </item>
  </channel>
</rss>