<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K3 SCST IAR Demo</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-SCST-IAR-Demo/m-p/1854215#M34619</link>
    <description>&lt;P&gt;Hi, I purchased SCST lib for Cortex M7, and i need to integrate it to my project which base on IAR compiler, but the library i purchased dosen't provide a IAR demo project, i don't kown how to dispatch each section of SCST in the address link file of IAR(*.ict). So is there a SCST demo project based on IAR?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I put section .m7_sctst_test_shell_data to ramblock in the link file, it encounterd an error after compiling "there was no reference to __iar_data_init3, but it is needed to initialize section .m7_sctst_test_shell_data..."&lt;/P&gt;</description>
    <pubDate>Fri, 26 Apr 2024 06:45:29 GMT</pubDate>
    <dc:creator>jhuang1</dc:creator>
    <dc:date>2024-04-26T06:45:29Z</dc:date>
    <item>
      <title>S32K3 SCST IAR Demo</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-SCST-IAR-Demo/m-p/1854215#M34619</link>
      <description>&lt;P&gt;Hi, I purchased SCST lib for Cortex M7, and i need to integrate it to my project which base on IAR compiler, but the library i purchased dosen't provide a IAR demo project, i don't kown how to dispatch each section of SCST in the address link file of IAR(*.ict). So is there a SCST demo project based on IAR?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I put section .m7_sctst_test_shell_data to ramblock in the link file, it encounterd an error after compiling "there was no reference to __iar_data_init3, but it is needed to initialize section .m7_sctst_test_shell_data..."&lt;/P&gt;</description>
      <pubDate>Fri, 26 Apr 2024 06:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-SCST-IAR-Demo/m-p/1854215#M34619</guid>
      <dc:creator>jhuang1</dc:creator>
      <dc:date>2024-04-26T06:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 SCST IAR Demo</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-SCST-IAR-Demo/m-p/1859439#M34972</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217679"&gt;@jhuang1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There is no IAR demo.&lt;/P&gt;
&lt;P&gt;But you can refer to the attached linker file and startup code.&lt;/P&gt;
&lt;P&gt;It seems you don't call __iar_data_init3&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 May 2024 06:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-SCST-IAR-Demo/m-p/1859439#M34972</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-05-06T06:45:15Z</dc:date>
    </item>
  </channel>
</rss>