<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: How to configure a input trigger for LPSPI in s32k ?</title>
    <link>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1853174#M34577</link>
    <description>&lt;P&gt;Please create a new thread if the question is not on the original subject of this thread.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
    <pubDate>Wed, 24 Apr 2024 07:04:41 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2024-04-24T07:04:41Z</dc:date>
    <item>
      <title>How to configure a input trigger for LPSPI in s32k ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1851157#M34451</link>
      <description>&lt;P&gt;Our project is configured/developed using EB Tresos.&lt;/P&gt;&lt;P&gt;Our idea is that there is a slave and when it wants to communicate with the master(our MCU). It will set a GPIO pin as high. So the master must do the data transfers as long as this pin is high. How to do this?&lt;/P&gt;&lt;P&gt;What are the important troubles that we may have to look for? Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 04:40:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1851157#M34451</guid>
      <dc:creator>Guna</dc:creator>
      <dc:date>2024-04-22T04:40:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure a input trigger for LPSPI in s32k ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1851632#M34499</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231069"&gt;@Guna&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Which version of the RTD drivers do you have?&lt;/P&gt;
&lt;P&gt;Spi Host Request feature is not supported in RTD 3.0.0 but it is supported in RTD 4.0.0.&lt;/P&gt;
&lt;P&gt;Refer to the RTD_SPI_UM.pdf&lt;/P&gt;
&lt;P&gt;Section 3.6.11 How to configure to use Spi Host Request feature.&lt;/P&gt;
&lt;P&gt;...\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Spi_TS_T40D34M40I0R0\doc\&lt;/P&gt;
&lt;P&gt;S32DS installation directory:&lt;/P&gt;
&lt;P&gt;c:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Spi_TS_T40D34M40I0R0\doc\&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 12:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1851632#M34499</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-04-22T12:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure a input trigger for LPSPI in s32k ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1852137#M34526</link>
      <description>&lt;P&gt;We are using 3.0.0 only. Any method u know on how to configure GPIO SPI interrupt request(Or Host req feature) in s32k358 . Presently we are configuring ICU driver for interrupt but the drawback is after every data transfer we have to manually look using software whether that GPIO is high, if yes again do the data transfer or end the transfer. In HREQ, i believe this part is totally handled by hardware.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 06:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1852137#M34526</guid>
      <dc:creator>Guna</dc:creator>
      <dc:date>2024-04-23T06:22:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure a input trigger for LPSPI in s32k ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1852487#M34544</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231069"&gt;@Guna&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, the LPSPI module supports HW HREQ.&lt;/P&gt;
&lt;P&gt;You can refer to the RTD 4.0.0 SPI driver.&lt;/P&gt;
&lt;P&gt;We don't have any GPIO solution for that, but you could enable interrupts of both edges.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 11:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1852487#M34544</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-04-23T11:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure a input trigger for LPSPI in s32k ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1853017#M34569</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have another query. I wanted to test SPI is working or not. So, I configured one of our boards as slave and another same board as master. But while configuring I encountered a problem in EBTresos saying Slave can only work in asynchronous transmission. So, I configured slave in Asynchronous mode. Please note that master is our main board it has to be synchronous mode and we configured slave to just test the master.&lt;/P&gt;&lt;P&gt;Two queries: -&lt;/P&gt;&lt;P&gt;1. Can we configure LPSPI as slave in synchronous mode?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. If not, then if we connect master and slave together--will it work(as the parameters are same only in master and slave, i only changed SpiPhyUnitMode from master to Slave and Unchecked SpiPhyUnitSync in Slave side)?&lt;/P&gt;&lt;P&gt;We are using&amp;nbsp;S32K3 Real-Time Drivers AUTOSAR 4.4 &amp;amp; R21-11 Version 3.0.0.&lt;/P&gt;&lt;P&gt;N.B refer image attached for reference.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 04:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1853017#M34569</guid>
      <dc:creator>Guna</dc:creator>
      <dc:date>2024-04-24T04:32:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure a input trigger for LPSPI in s32k ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1853174#M34577</link>
      <description>&lt;P&gt;Please create a new thread if the question is not on the original subject of this thread.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 07:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-configure-a-input-trigger-for-LPSPI-in-s32k/m-p/1853174#M34577</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-04-24T07:04:41Z</dc:date>
    </item>
  </channel>
</rss>