<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS project folder structure in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32DS-project-folder-structure/m-p/1853097#M34574</link>
    <description>Good to know, thanks for the answer Julián.</description>
    <pubDate>Wed, 24 Apr 2024 06:07:57 GMT</pubDate>
    <dc:creator>JCastro</dc:creator>
    <dc:date>2024-04-24T06:07:57Z</dc:date>
    <item>
      <title>S32DS project folder structure</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-project-folder-structure/m-p/1852540#M34550</link>
      <description>&lt;P&gt;Hello, I'm trying to generate a S32DS project with a custom folder project structure, I generate the project from the hello world example for the S32K311 MCU. I want the following structure:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;- app/
- libs/
- board/
    - S32K311/
        - generate/
        - S32K311.mex
        - rtd/
        - ...&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The project builds successfully, but when I update the generated code (using the S32K311.mex) the RTD folder appears in the root of the project and this include -&amp;gt; "&lt;EM&gt;../RTD/include&lt;/EM&gt;".&lt;/P&gt;&lt;P&gt;Is there any way to avoid this undesired behavior?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 13:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-project-folder-structure/m-p/1852540#M34550</guid>
      <dc:creator>JCastro</dc:creator>
      <dc:date>2024-04-23T13:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS project folder structure</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-project-folder-structure/m-p/1852704#M34555</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231381"&gt;@JCastro&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Unfortunately, it is not possible to modify where the code is generated, but you can export the source files:&lt;/P&gt;
&lt;P&gt;"&lt;EM&gt;Right click &amp;gt; Export... &amp;gt; S32 Configuration Tools &amp;gt; Export Source Files"&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1713891719947.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275328i1351DAF0088A44D4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1713891719947.png" alt="Julin_AragnM_0-1713891719947.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_0-1713891719947.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You could also add a script to run as pre/post-build steps, so the desired folders are generated:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_2-1713891912319.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275331i64D6789F22EB0422/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_2-1713891912319.png" alt="Julin_AragnM_2-1713891912319.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_2-1713891912319.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 17:05:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-project-folder-structure/m-p/1852704#M34555</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-04-23T17:05:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS project folder structure</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-project-folder-structure/m-p/1853097#M34574</link>
      <description>Good to know, thanks for the answer Julián.</description>
      <pubDate>Wed, 24 Apr 2024 06:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-project-folder-structure/m-p/1853097#M34574</guid>
      <dc:creator>JCastro</dc:creator>
      <dc:date>2024-04-24T06:07:57Z</dc:date>
    </item>
  </channel>
</rss>