<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: [S32K146] SPI#2 doesn't receive any data from Rx FIFO</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-SPI-2-doesn-t-receive-any-data-from-Rx-FIFO/m-p/845721#M3454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;You configured 128-bit long frame (TCR_FRAMESZ). &lt;BR /&gt;Can you try with a short frame first?&lt;BR /&gt;Can you share your code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jul 2018 15:25:23 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-07-25T15:25:23Z</dc:date>
    <item>
      <title>[S32K146] SPI#2 doesn't receive any data from Rx FIFO</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-SPI-2-doesn-t-receive-any-data-from-Rx-FIFO/m-p/845720#M3453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear NXP team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my automotive project, the S32K146 controls the ADSP via SPI.&lt;/P&gt;&lt;P&gt;The SPI#2 (PTB25,27,28,29) is used for it and I can see the valid signals on the PTB28 (LPSPI2_SIN).&lt;/P&gt;&lt;P&gt;But the data from RX FIFO is always empty (0x00).&lt;/P&gt;&lt;P&gt;I've checked the PINMUX configuration for them, but there's no problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a register dump for SPI#2.&lt;/P&gt;&lt;P&gt;Could you check whether there is a problem on it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;========== PINMUX for SPI#2 ==========&lt;BR /&gt;PORTB-&amp;gt;PCR[25] = 0x00000500&lt;BR /&gt;PORTB-&amp;gt;PCR[27] = 0x00000500&lt;BR /&gt;PORTB-&amp;gt;PCR[28] = 0x00000500&lt;BR /&gt;PORTB-&amp;gt;PCR[29] = 0x00000500&lt;BR /&gt;=====================================&lt;BR /&gt;========== SPI#2 registers ==========&lt;BR /&gt;LPSPI2-&amp;gt;PARAM = 0x00000202&lt;BR /&gt;LPSPI2-&amp;gt;CR = 0x00000009&lt;BR /&gt;LPSPI2-&amp;gt;SR = 0x00000001&lt;BR /&gt;LPSPI2-&amp;gt;IER = 0x00000000&lt;BR /&gt;LPSPI2-&amp;gt;DER = 0x00000000&lt;BR /&gt;LPSPI2-&amp;gt;CFGR0 = 0x00000000&lt;BR /&gt;LPSPI2-&amp;gt;CFGR1 = 0x00000001&lt;BR /&gt;LPSPI2-&amp;gt;DMR0 = 0x00000000&lt;BR /&gt;LPSPI2-&amp;gt;DMR1 = 0x00000000&lt;BR /&gt;LPSPI2-&amp;gt;CCR = 0xdcdcdc6e&lt;BR /&gt;LPSPI2-&amp;gt;FCR = 0x00020001&lt;BR /&gt;LPSPI2-&amp;gt;FSR = 0x00000000&lt;BR /&gt;LPSPI2-&amp;gt;TCR = 0x0000007f&lt;BR /&gt;LPSPI2-&amp;gt;RSR = 0x00000002&lt;BR /&gt;=====================================&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 05:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-SPI-2-doesn-t-receive-any-data-from-Rx-FIFO/m-p/845720#M3453</guid>
      <dc:creator>yongho_shin</dc:creator>
      <dc:date>2018-07-24T05:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K146] SPI#2 doesn't receive any data from Rx FIFO</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-SPI-2-doesn-t-receive-any-data-from-Rx-FIFO/m-p/845721#M3454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;You configured 128-bit long frame (TCR_FRAMESZ). &lt;BR /&gt;Can you try with a short frame first?&lt;BR /&gt;Can you share your code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 15:25:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-SPI-2-doesn-t-receive-any-data-from-Rx-FIFO/m-p/845721#M3454</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-07-25T15:25:23Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K146] SPI#2 doesn't receive any data from Rx FIFO</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-SPI-2-doesn-t-receive-any-data-from-Rx-FIFO/m-p/845722#M3455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried with short frame sizes - 8bits, 16bits, 32bits, but it also has same problem.&lt;/P&gt;&lt;P&gt;Currently I'm testing with the reference code of the S32K SDK and will let you know the result.&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Yongho Shin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2018 00:42:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-SPI-2-doesn-t-receive-any-data-from-Rx-FIFO/m-p/845722#M3455</guid>
      <dc:creator>yongho_shin</dc:creator>
      <dc:date>2018-07-27T00:42:08Z</dc:date>
    </item>
  </channel>
</rss>