<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Multiple Port LSPSPI</title>
    <link>https://community.nxp.com/t5/S32K/Multiple-Port-LSPSPI/m-p/1852278#M34534</link>
    <description>&lt;P&gt;I am trying to initiate an SPI transmission over these ports:&amp;nbsp;&lt;/P&gt;&lt;P&gt;SCLK: PTC15&lt;/P&gt;&lt;P&gt;MISO: PTE16&lt;/P&gt;&lt;P&gt;MOSI: PTC1&lt;/P&gt;&lt;P&gt;CS: PTC14&lt;BR /&gt;&lt;BR /&gt;but the CS isn't working at all. But if I change CS to PCS3 then it works, which is not cool because I&amp;nbsp; already have my PCB pinout to PTC14.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Another Problem is that I cant seem to see any data&amp;nbsp; on MISO: PTE16. Should I be considering another art of port initialization when I have 2 Ports?&amp;nbsp;&lt;BR /&gt;I init them like this:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;PCC-&amp;gt;PCCn[PCC_PORTE_INDEX ]|=PCC_PCCn_CGC_MASK; /* Enable clock for PORTE */&lt;BR /&gt;&amp;nbsp;PCC-&amp;gt;PCCn[PCC_PORTC_INDEX ]|=PCC_PCCn_CGC_MASK; /* Enable clock for PORTC */&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Apr 2024 08:01:04 GMT</pubDate>
    <dc:creator>Khaledag</dc:creator>
    <dc:date>2024-04-23T08:01:04Z</dc:date>
    <item>
      <title>Multiple Port LSPSPI</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-Port-LSPSPI/m-p/1852278#M34534</link>
      <description>&lt;P&gt;I am trying to initiate an SPI transmission over these ports:&amp;nbsp;&lt;/P&gt;&lt;P&gt;SCLK: PTC15&lt;/P&gt;&lt;P&gt;MISO: PTE16&lt;/P&gt;&lt;P&gt;MOSI: PTC1&lt;/P&gt;&lt;P&gt;CS: PTC14&lt;BR /&gt;&lt;BR /&gt;but the CS isn't working at all. But if I change CS to PCS3 then it works, which is not cool because I&amp;nbsp; already have my PCB pinout to PTC14.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Another Problem is that I cant seem to see any data&amp;nbsp; on MISO: PTE16. Should I be considering another art of port initialization when I have 2 Ports?&amp;nbsp;&lt;BR /&gt;I init them like this:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;PCC-&amp;gt;PCCn[PCC_PORTE_INDEX ]|=PCC_PCCn_CGC_MASK; /* Enable clock for PORTE */&lt;BR /&gt;&amp;nbsp;PCC-&amp;gt;PCCn[PCC_PORTC_INDEX ]|=PCC_PCCn_CGC_MASK; /* Enable clock for PORTC */&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 08:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-Port-LSPSPI/m-p/1852278#M34534</guid>
      <dc:creator>Khaledag</dc:creator>
      <dc:date>2024-04-23T08:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Port LSPSPI</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-Port-LSPSPI/m-p/1852457#M34543</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;if a PTC14 pin is configured to select LPSPI2 PCS0 function and LPSPI2 TCR is selecting PCS0, then you should see signal on it.&lt;/P&gt;&lt;P&gt;If PTE16 is used as SIN then PTE port clock have to be enabled too.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 10:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-Port-LSPSPI/m-p/1852457#M34543</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-04-23T10:58:06Z</dc:date>
    </item>
  </channel>
</rss>