<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Bootloader to application jump issue in S32k344 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Bootloader-to-application-jump-issue-in-S32k344/m-p/1851301#M34471</link>
    <description>&lt;P&gt;Hi, I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions. 1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. I need the reply as soon as possible since I have to send a project very soon.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_0-1713768134672.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274900i8EE1C99FA1D258B4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_0-1713768134672.png" alt="JonAnder_Amante_0-1713768134672.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_1-1713768134675.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274899i7D6B281D3F3876FD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_1-1713768134675.png" alt="JonAnder_Amante_1-1713768134675.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_2-1713768134676.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274898iABD71042DD08AC0B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_2-1713768134676.png" alt="JonAnder_Amante_2-1713768134676.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_3-1713768134680.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274902i6662D510490D3EF2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_3-1713768134680.png" alt="JonAnder_Amante_3-1713768134680.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_4-1713768134679.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274901i88C80C0C1F7A5DAF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_4-1713768134679.png" alt="JonAnder_Amante_4-1713768134679.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for all,&lt;/P&gt;</description>
    <pubDate>Mon, 22 Apr 2024 06:42:33 GMT</pubDate>
    <dc:creator>JonAnder_Amante</dc:creator>
    <dc:date>2024-04-22T06:42:33Z</dc:date>
    <item>
      <title>Bootloader to application jump issue in S32k344</title>
      <link>https://community.nxp.com/t5/S32K/Bootloader-to-application-jump-issue-in-S32k344/m-p/1490921#M16444</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Error SystemInit in system.c file&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 08:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Bootloader-to-application-jump-issue-in-S32k344/m-p/1490921#M16444</guid>
      <dc:creator>zhangyang123</dc:creator>
      <dc:date>2022-07-18T08:36:06Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader to application jump issue in S32k344</title>
      <link>https://community.nxp.com/t5/S32K/Bootloader-to-application-jump-issue-in-S32k344/m-p/1491634#M16489</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203809"&gt;@zhangyang123&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you elaborate on the description?&lt;/P&gt;
&lt;P&gt;I can't tell what the issue is from the description.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 08:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Bootloader-to-application-jump-issue-in-S32k344/m-p/1491634#M16489</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-07-19T08:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader to application jump issue in S32k344</title>
      <link>https://community.nxp.com/t5/S32K/Bootloader-to-application-jump-issue-in-S32k344/m-p/1851301#M34471</link>
      <description>&lt;P&gt;Hi, I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions. 1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. I need the reply as soon as possible since I have to send a project very soon.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_0-1713768134672.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274900i8EE1C99FA1D258B4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_0-1713768134672.png" alt="JonAnder_Amante_0-1713768134672.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_1-1713768134675.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274899i7D6B281D3F3876FD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_1-1713768134675.png" alt="JonAnder_Amante_1-1713768134675.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_2-1713768134676.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274898iABD71042DD08AC0B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_2-1713768134676.png" alt="JonAnder_Amante_2-1713768134676.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_3-1713768134680.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274902i6662D510490D3EF2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_3-1713768134680.png" alt="JonAnder_Amante_3-1713768134680.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_4-1713768134679.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274901i88C80C0C1F7A5DAF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_4-1713768134679.png" alt="JonAnder_Amante_4-1713768134679.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for all,&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 06:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Bootloader-to-application-jump-issue-in-S32k344/m-p/1851301#M34471</guid>
      <dc:creator>JonAnder_Amante</dc:creator>
      <dc:date>2024-04-22T06:42:33Z</dc:date>
    </item>
  </channel>
</rss>