<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K 3.4ver CAN_Node</title>
    <link>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849370#M34330</link>
    <description>&lt;P&gt;I wondered that&lt;/P&gt;&lt;P&gt;if erased CAN Source, Errors not occured.&lt;/P&gt;&lt;P&gt;but if add CAN Source, paralyzed all CAN_Node associated to CAN_BUS.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If our CAN node can influenced on CAN_BUS without TX ??&lt;BR /&gt;(our CAN source code has only RX)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;On the other side, ARM CAN source doesn't occur error.&lt;/P&gt;</description>
    <pubDate>Thu, 18 Apr 2024 00:55:48 GMT</pubDate>
    <dc:creator>mumumilmil</dc:creator>
    <dc:date>2024-04-18T00:55:48Z</dc:date>
    <item>
      <title>S32K 3.4ver CAN_Node</title>
      <link>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849370#M34330</link>
      <description>&lt;P&gt;I wondered that&lt;/P&gt;&lt;P&gt;if erased CAN Source, Errors not occured.&lt;/P&gt;&lt;P&gt;but if add CAN Source, paralyzed all CAN_Node associated to CAN_BUS.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If our CAN node can influenced on CAN_BUS without TX ??&lt;BR /&gt;(our CAN source code has only RX)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;On the other side, ARM CAN source doesn't occur error.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Apr 2024 00:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849370#M34330</guid>
      <dc:creator>mumumilmil</dc:creator>
      <dc:date>2024-04-18T00:55:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K 3.4ver CAN_Node</title>
      <link>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849375#M34331</link>
      <description>&lt;P&gt;I have been&amp;nbsp;a&lt;SPAN&gt;nalyzing our 3.4ver source code..&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;To find solution, please give me your opinion&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Apr 2024 01:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849375#M34331</guid>
      <dc:creator>mumumilmil</dc:creator>
      <dc:date>2024-04-18T01:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K 3.4ver CAN_Node</title>
      <link>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849563#M34335</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;would be great to know how such paralyze looks like. Ideally check for errors detected on nodes and measure your node TXD/RXD and CAN signals.&lt;BR /&gt;Even if node is not transmitting a message it receives frames and ACKs it back and in case of any error detected it sends error frame.&lt;BR /&gt;If you need not TX on node you can try to use LOM (Listen Only Mode).&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 18 Apr 2024 06:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849563#M34335</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-04-18T06:28:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K 3.4ver CAN_Node</title>
      <link>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849669#M34340</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Are you saying that I can receive it as an RX signal and reply the error frame without sending the TX signal from NODE?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;and&amp;nbsp;&lt;SPAN&gt;Does the error frame sent over the ACK signal also cause errors on other nodes of CAN_BUS?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Apr 2024 08:17:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1849669#M34340</guid>
      <dc:creator>mumumilmil</dc:creator>
      <dc:date>2024-04-18T08:17:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K 3.4ver CAN_Node</title>
      <link>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1850649#M34404</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;FlexCAN module behaves as per CAN standard so you can refer to it for info about error handling.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 19 Apr 2024 11:08:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-3-4ver-CAN-Node/m-p/1850649#M34404</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-04-19T11:08:22Z</dc:date>
    </item>
  </channel>
</rss>