<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRTD naming question</title>
    <link>https://community.nxp.com/t5/S32K/RTD-naming-question/m-p/1844264#M34013</link>
    <description>&lt;P&gt;Hi NXP experts,&lt;/P&gt;&lt;P&gt;I am a little confused with the naming of the RTDs,&amp;nbsp;&lt;/P&gt;&lt;P&gt;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 4.0.0 P19&lt;/P&gt;&lt;P&gt;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 4.0.0 P12&lt;/P&gt;&lt;P&gt;S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 4.0.0 HF01&lt;/P&gt;&lt;P&gt;S32K388 Real-Time Drivers Version 4.0.0 CD01&lt;BR /&gt;Seems P = Patch, HF = Hot Fix, CD = Code Drop, then what's the difference between P/HF/CD?&amp;nbsp;&lt;BR /&gt;the newest RTD should be P , HF, or CD?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 10 Apr 2024 18:45:46 GMT</pubDate>
    <dc:creator>focusdoit</dc:creator>
    <dc:date>2024-04-10T18:45:46Z</dc:date>
    <item>
      <title>RTD naming question</title>
      <link>https://community.nxp.com/t5/S32K/RTD-naming-question/m-p/1844264#M34013</link>
      <description>&lt;P&gt;Hi NXP experts,&lt;/P&gt;&lt;P&gt;I am a little confused with the naming of the RTDs,&amp;nbsp;&lt;/P&gt;&lt;P&gt;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 4.0.0 P19&lt;/P&gt;&lt;P&gt;S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 4.0.0 P12&lt;/P&gt;&lt;P&gt;S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 4.0.0 HF01&lt;/P&gt;&lt;P&gt;S32K388 Real-Time Drivers Version 4.0.0 CD01&lt;BR /&gt;Seems P = Patch, HF = Hot Fix, CD = Code Drop, then what's the difference between P/HF/CD?&amp;nbsp;&lt;BR /&gt;the newest RTD should be P , HF, or CD?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 10 Apr 2024 18:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTD-naming-question/m-p/1844264#M34013</guid>
      <dc:creator>focusdoit</dc:creator>
      <dc:date>2024-04-10T18:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: RTD naming question</title>
      <link>https://community.nxp.com/t5/S32K/RTD-naming-question/m-p/1844885#M34036</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes it is:&lt;/P&gt;
&lt;P&gt;P- Patch - comes with full RTD package as it is a release&lt;/P&gt;
&lt;P&gt;HF - Only the fixed modules as it is not a release&lt;/P&gt;
&lt;P&gt;CD - Code drop&amp;nbsp; - All software included in this release has Code Drop quality status in terms of testing and of quality documentation. Code Drop qualified releases are not fully tested and contain partial feature set. It is not intended to be used in production.&lt;/P&gt;
&lt;P&gt;Always refer to the release notes of that particular package. There is a detailed description.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 11 Apr 2024 06:58:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTD-naming-question/m-p/1844885#M34036</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-04-11T06:58:05Z</dc:date>
    </item>
  </channel>
</rss>