<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN IRQHANDLER in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-IRQHANDLER/m-p/597744#M34</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to use CAN0_ORed_0_15_MB_IRQHandler or CAN0_ORed_16_31_MB_IRQHandler depending on used MB. Moreover, the interrupt controller have to be initialized and interrupt enabled within the FlexCAN module for desired MB using the IMASK1 register.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is the modified FlexCAN example which is included within an S32DS13 intallation.&lt;/P&gt;&lt;P&gt;Loopback mode is enabled (can be tested on single board) and interrupt for MB4 is added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Mar 2017 12:55:34 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-03-22T12:55:34Z</dc:date>
    <item>
      <title>CAN IRQHANDLER</title>
      <link>https://community.nxp.com/t5/S32K/CAN-IRQHANDLER/m-p/597743#M33</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How I use CAN interupt to receive data? &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Do I have to use CAN0_ORed_IRQHandler?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Because without using interrupts I'm losing data.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Does anyone have an example?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Thanks.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Mar 2017 14:29:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-IRQHANDLER/m-p/597743#M33</guid>
      <dc:creator>lohrsistemas</dc:creator>
      <dc:date>2017-03-18T14:29:39Z</dc:date>
    </item>
    <item>
      <title>Re: CAN IRQHANDLER</title>
      <link>https://community.nxp.com/t5/S32K/CAN-IRQHANDLER/m-p/597744#M34</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to use CAN0_ORed_0_15_MB_IRQHandler or CAN0_ORed_16_31_MB_IRQHandler depending on used MB. Moreover, the interrupt controller have to be initialized and interrupt enabled within the FlexCAN module for desired MB using the IMASK1 register.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is the modified FlexCAN example which is included within an S32DS13 intallation.&lt;/P&gt;&lt;P&gt;Loopback mode is enabled (can be tested on single board) and interrupt for MB4 is added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 12:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-IRQHANDLER/m-p/597744#M34</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-03-22T12:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: CAN IRQHANDLER</title>
      <link>https://community.nxp.com/t5/S32K/CAN-IRQHANDLER/m-p/597745#M35</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Hi Petr,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Thanks for your feedback.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;It's working here.&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;Regards.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 14:09:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-IRQHANDLER/m-p/597745#M35</guid>
      <dc:creator>lohrsistemas</dc:creator>
      <dc:date>2017-03-22T14:09:29Z</dc:date>
    </item>
  </channel>
</rss>