<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K I/O SPEED too slow in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842363#M3396</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I think you can get better results with LMEM Cache:&lt;/P&gt;&lt;P&gt;LMEM-&amp;gt;PCCCR = 0x85000001;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Aug 2018 10:54:04 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-08-17T10:54:04Z</dc:date>
    <item>
      <title>S32K I/O SPEED too slow</title>
      <link>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842360#M3393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HELLO，R&lt;SPAN style="color: #333333; background-color: #ffffff; font-weight: 200; font-size: 14.000000953674316px;"&gt;ecently I discovered &amp;nbsp;&lt;/SPAN&gt;S32K's IO speed is not as fast as i wish。The CPU frq is 112Mhz，bus frq is 56Mhz。The IO speed is 130ns，that is 7.7MHZ。I was not use SDK but directly write the register &amp;nbsp;PDOR.As usually, IO Speed can reach the half of Bus frq.That is when bus frq is 56MHZ,io speed can reach 26Mhz.But S32K's is just 7.7MHz.Can S32K's io speed faster?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 03:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842360#M3393</guid>
      <dc:creator>zhengjianfei</dc:creator>
      <dc:date>2018-08-10T03:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32K I/O SPEED too slow</title>
      <link>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842361#M3394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could you please tell me the use case of such an implementation? If you want to generate a PWM signal or toggle GPIO for some timing purposes, you can use hardware peripherals.&lt;/P&gt;&lt;P&gt;There are many variables that influence the frequency. Number of instructions, prefetching, wait states on crossbar switch...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 10:53:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842361#M3394</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-08-16T10:53:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K I/O SPEED too slow</title>
      <link>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842362#M3395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use GPIO to drive a 16bit LCD。So I need GPIO as fast as it can。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 01:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842362#M3395</guid>
      <dc:creator>zhengjianfei</dc:creator>
      <dc:date>2018-08-17T01:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K I/O SPEED too slow</title>
      <link>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842363#M3396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I think you can get better results with LMEM Cache:&lt;/P&gt;&lt;P&gt;LMEM-&amp;gt;PCCCR = 0x85000001;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2018 10:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-I-O-SPEED-too-slow/m-p/842363#M3396</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-08-17T10:54:04Z</dc:date>
    </item>
  </channel>
</rss>