<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: s32k mcal Spi</title>
    <link>https://community.nxp.com/t5/S32K/s32k-mcal-Spi/m-p/1840950#M33831</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194181"&gt;@Higgs_Boson&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;&lt;EM&gt;SrcDataBufferPtr&lt;/EM&gt; and&amp;nbsp;&lt;EM&gt;DesDataBufferPtr&lt;/EM&gt;:&amp;nbsp;Pointer to source/destination data buffer. These parameters have defined as&amp;nbsp;&lt;EM&gt;Spi_DataBufferType&lt;/EM&gt;, which is uint8 for each element in it buffer.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;&lt;EM&gt;Length&lt;/EM&gt;: Number of data elements in above Src/Des data buffer.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;SPAN class="uiOutputText"&gt;The setting of&amp;nbsp;SpiDataWidth is the width of each transmitted data unit. For example, 16 bits mean that each time transmit, the SPI driver will transmit 16bits at a&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;time. So&lt;SPAN class="uiOutputText"&gt;, you still need to setup Length in SetupEB as 2 for 16bits Framesize.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;SPAN class="uiOutputText"&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Apr 2024 18:16:19 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-04-04T18:16:19Z</dc:date>
    <item>
      <title>s32k mcal Spi</title>
      <link>https://community.nxp.com/t5/S32K/s32k-mcal-Spi/m-p/1839986#M33761</link>
      <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;The autosar api Spi_SetupEB() in s32k mcal we have use in project, we wonder the passing parameter &amp;nbsp;'Length' Meaning. In Autosar Description, it means 'data of element'. it means u8 or u16 or u32? How is it define in nxp s32k mcal?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="IMG_0148.jpeg" style="width: 1037px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271763i1CE9929B48A0D0CE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="IMG_0148.jpeg" alt="IMG_0148.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 07:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k-mcal-Spi/m-p/1839986#M33761</guid>
      <dc:creator>Higgs_Boson</dc:creator>
      <dc:date>2024-04-03T07:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: s32k mcal Spi</title>
      <link>https://community.nxp.com/t5/S32K/s32k-mcal-Spi/m-p/1840950#M33831</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194181"&gt;@Higgs_Boson&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;&lt;EM&gt;SrcDataBufferPtr&lt;/EM&gt; and&amp;nbsp;&lt;EM&gt;DesDataBufferPtr&lt;/EM&gt;:&amp;nbsp;Pointer to source/destination data buffer. These parameters have defined as&amp;nbsp;&lt;EM&gt;Spi_DataBufferType&lt;/EM&gt;, which is uint8 for each element in it buffer.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="uiOutputText"&gt;&lt;EM&gt;Length&lt;/EM&gt;: Number of data elements in above Src/Des data buffer.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;SPAN class="uiOutputText"&gt;The setting of&amp;nbsp;SpiDataWidth is the width of each transmitted data unit. For example, 16 bits mean that each time transmit, the SPI driver will transmit 16bits at a&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;time. So&lt;SPAN class="uiOutputText"&gt;, you still need to setup Length in SetupEB as 2 for 16bits Framesize.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&lt;SPAN class="uiOutputText"&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Apr 2024 18:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k-mcal-Spi/m-p/1840950#M33831</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-04-04T18:16:19Z</dc:date>
    </item>
  </channel>
</rss>