<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Port Pin Configuration Error in Peripherals in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1830197#M33111</link>
    <description>&lt;P&gt;Thanks for the reply first.&lt;/P&gt;&lt;P&gt;What if we use RTD 2.0.1?&amp;nbsp;&lt;/P&gt;&lt;P&gt;We tried RTD 2.0.0, 2.0.1, shall we go for 2.0.3 ? our base version is installed with 2.0.1 version. we are working on one of the base version (already implemented by others).&lt;/P&gt;&lt;P&gt;also is there procedure to migrate RTD 2.0.1 to other versions ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if all these above are not an issue, if we moved to 2.0.3 ? there will be any issue will takes place?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or still we can go for it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 18 Mar 2024 09:57:30 GMT</pubDate>
    <dc:creator>NadipalliLTTS</dc:creator>
    <dc:date>2024-03-18T09:57:30Z</dc:date>
    <item>
      <title>Port Pin Configuration Error in Peripherals</title>
      <link>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1829043#M33026</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;Currently We are working on Port pin configuration of S32K312 in S32 Design studio 3.4 V&lt;/P&gt;&lt;P&gt;While configuring pins i am getting Peripherals error While clicking on Update Code button, it was showing as error as below. can someone help how to proceed here, in order to fix this error. While updating the Pin configuration we have tried in two ways. One way is we directly updated the pins in &lt;STRONG&gt;&lt;U&gt;Pins section&lt;/U&gt;&lt;/STRONG&gt;. the second way is we directly opened &lt;U&gt;&lt;STRONG&gt;Peripherals&lt;/STRONG&gt; &lt;/U&gt;tool. in Both configurations it was showing the error. Kindly help how to proceed here.&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Peripheral_error.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268593iE6BC6D686F0345E1/image-size/large?v=v2&amp;amp;px=999" role="button" title="Peripheral_error.jpg" alt="Peripheral_error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 05:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1829043#M33026</guid>
      <dc:creator>NadipalliLTTS</dc:creator>
      <dc:date>2024-03-15T05:16:00Z</dc:date>
    </item>
    <item>
      <title>Re: Port Pin Configuration Error in Peripherals</title>
      <link>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1830168#M33108</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;There are a lots of MCAL High Level Driver based examples in S32K3 RTD 2.0.3. I will not encounter any errors when Update Code in the Spi_Transfer_S32K312_RTD203 example that I imported. You don't need to use the &lt;EM&gt;Pins tool&lt;/EM&gt; of S32CT, just configure those pins in &lt;STRONG&gt;Port Configuration[MCAL]&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Port Configuration[MCAL].png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268931iC6C725AF10F6E8B3/image-size/large?v=v2&amp;amp;px=999" role="button" title="Port Configuration[MCAL].png" alt="Port Configuration[MCAL].png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 18 Mar 2024 09:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1830168#M33108</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-03-18T09:40:57Z</dc:date>
    </item>
    <item>
      <title>Re: Port Pin Configuration Error in Peripherals</title>
      <link>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1830197#M33111</link>
      <description>&lt;P&gt;Thanks for the reply first.&lt;/P&gt;&lt;P&gt;What if we use RTD 2.0.1?&amp;nbsp;&lt;/P&gt;&lt;P&gt;We tried RTD 2.0.0, 2.0.1, shall we go for 2.0.3 ? our base version is installed with 2.0.1 version. we are working on one of the base version (already implemented by others).&lt;/P&gt;&lt;P&gt;also is there procedure to migrate RTD 2.0.1 to other versions ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if all these above are not an issue, if we moved to 2.0.3 ? there will be any issue will takes place?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or still we can go for it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Mar 2024 09:57:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1830197#M33111</guid>
      <dc:creator>NadipalliLTTS</dc:creator>
      <dc:date>2024-03-18T09:57:30Z</dc:date>
    </item>
    <item>
      <title>Re: Port Pin Configuration Error in Peripherals</title>
      <link>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1830238#M33114</link>
      <description>&lt;P&gt;If the project is received from others. Please check the S32K3&amp;nbsp;Build Version of that project. For example: I imported Spi_Transfer_S32K312 of RTD 2.0.1, there you will see the version:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K3 RTD Build Version.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268950i2BB957A2976E9B1F/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K3 RTD Build Version.png" alt="S32K3 RTD Build Version.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Mar 2024 10:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Port-Pin-Configuration-Error-in-Peripherals/m-p/1830238#M33114</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-03-18T10:42:49Z</dc:date>
    </item>
  </channel>
</rss>