<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344 PIT timer callback function not working after SPI send data in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829173#M33035</link>
    <description>&lt;P&gt;Hi Support Team,&lt;/P&gt;&lt;P&gt;Because you provide test project is based on RTD 3.0.0, I install it and test your project. It works fine.&lt;/P&gt;&lt;P&gt;Then I retry my project it works fine too without any modification.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 15 Mar 2024 08:01:44 GMT</pubDate>
    <dc:creator>Steven_Cho</dc:creator>
    <dc:date>2024-03-15T08:01:44Z</dc:date>
    <item>
      <title>S32K344 PIT timer callback function not working after SPI send data</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1828924#M33017</link>
      <description>&lt;P&gt;Hi Support Team,&lt;/P&gt;&lt;P&gt;I set a PIT timer to enter the callback function once every 10ms. It base on&amp;nbsp; SW32K3_RTD_4.4_2.0.0.&lt;/P&gt;&lt;P&gt;When I use Lpspi_Ip_SyncTransmit to send 2 bytes, the timer works fine.&lt;BR /&gt;But the timer doesn't work after I send 30 bytes using Lpspi_Ip_SyncTransmit.&lt;/P&gt;&lt;P&gt;Can you tell me why this happened?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 01:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1828924#M33017</guid>
      <dc:creator>Steven_Cho</dc:creator>
      <dc:date>2024-03-15T01:37:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 PIT timer callback function not working after SPI send data</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1828967#M33022</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Steven_Cho" target="_blank"&gt;Hi@Steven_Cho&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The synchronization operate will block the current thread until the function is executed before continuing other operations, so make sure there is enough time to complete the current transfer.&lt;BR /&gt;You can try extending the PIT timing time and then test again&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 03:04:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1828967#M33022</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-15T03:04:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 PIT timer callback function not working after SPI send data</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829065#M33028</link>
      <description>&lt;P&gt;Hi Support Team,&lt;/P&gt;&lt;P&gt;I try to use Pit_Ip_StartChannel to extend 1 sec but still not work.&lt;/P&gt;&lt;P&gt;Should I change spi transmit method to&amp;nbsp;Lpspi_Ip_AsyncTransmit?&lt;/P&gt;&lt;P&gt;If yes, how to use&amp;nbsp;Lpspi_Ip_AsyncTransmit to send data? Could you give me a example?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 05:57:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829065#M33028</guid>
      <dc:creator>Steven_Cho</dc:creator>
      <dc:date>2024-03-15T05:57:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 PIT timer callback function not working after SPI send data</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829083#M33030</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Steven_Cho" target="_blank"&gt;Hi@Steven_Cho&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;you can sent me your project and i will help you check it.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 06:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829083#M33030</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-15T06:15:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 PIT timer callback function not working after SPI send data</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829122#M33034</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Steven_Cho" target="_blank"&gt;Hi@Steven_Cho&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I made a very simple routine, you can refer to it and test it. I did not have the problem you mentioned.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 07:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829122#M33034</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-15T07:03:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 PIT timer callback function not working after SPI send data</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829173#M33035</link>
      <description>&lt;P&gt;Hi Support Team,&lt;/P&gt;&lt;P&gt;Because you provide test project is based on RTD 3.0.0, I install it and test your project. It works fine.&lt;/P&gt;&lt;P&gt;Then I retry my project it works fine too without any modification.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 08:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-PIT-timer-callback-function-not-working-after-SPI-send/m-p/1829173#M33035</guid>
      <dc:creator>Steven_Cho</dc:creator>
      <dc:date>2024-03-15T08:01:44Z</dc:date>
    </item>
  </channel>
</rss>