<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Create a delay in s32k118 using gpt start timer</title>
    <link>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1828510#M33001</link>
    <description>&lt;P&gt;Dear Julian&lt;/P&gt;&lt;P&gt;I am trying to debug to check whether isr has come up or not, while loop is executing once.but going to default isr.any suggestion how to check interrupt is running or not .&lt;/P&gt;</description>
    <pubDate>Thu, 14 Mar 2024 13:17:34 GMT</pubDate>
    <dc:creator>Ashish4525</dc:creator>
    <dc:date>2024-03-14T13:17:34Z</dc:date>
    <item>
      <title>Create a delay in s32k118 using gpt start timer</title>
      <link>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1827153#M32914</link>
      <description>&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;I am trying to build delay of 1 ms using GPT start timer and I am using LPIT0ch0, I have enable even LPITIrqn via NVICISER0.&lt;/P&gt;&lt;P&gt;I have called enableiRq and passed lpit as arguments.please go through my code once.&lt;/P&gt;&lt;P&gt;Can anyone help me?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 12:03:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1827153#M32914</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-03-13T12:03:54Z</dc:date>
    </item>
    <item>
      <title>Re: Create a delay in s32k118 using gpt start timer</title>
      <link>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1827609#M32932</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225256"&gt;@Ashish4525&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I see you have posted a similar thread on the community; I will try to answer them both on this post.&lt;/P&gt;
&lt;P&gt;You are using EB Tresos along with SW32K1_RTD, is this correct? If so, please take a look into the EB examples for the S32K118;&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Ftm_Gpt_Example_S32K118&lt;/LI&gt;
&lt;LI&gt;Gpt_example_S32K118&lt;/LI&gt;
&lt;LI&gt;Lpit_Gpt_Example_S32K118&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The Lpit_Gpt_Example_S32K118 application uses the IP layer functionality to trigger a timer interrupt. Notification function increase a count variable by 1 and toggle state pin LED on board.&lt;/P&gt;
&lt;P&gt;Please try this example for the GPT Pit interruption.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 21:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1827609#M32932</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-03-13T21:37:57Z</dc:date>
    </item>
    <item>
      <title>Re: Create a delay in s32k118 using gpt start timer</title>
      <link>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1828005#M32960</link>
      <description>&lt;P&gt;Dear julian&lt;/P&gt;&lt;P&gt;I am trying to make a delay using autosar i have generated all the files for mcu gpt and port so can you tell me api to call in main function,so that I come to know delay is working.&lt;/P&gt;&lt;P&gt;with regards&lt;/P&gt;&lt;P&gt;Ashish&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 05:07:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1828005#M32960</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-03-14T05:07:02Z</dc:date>
    </item>
    <item>
      <title>Re: Create a delay in s32k118 using gpt start timer</title>
      <link>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1828510#M33001</link>
      <description>&lt;P&gt;Dear Julian&lt;/P&gt;&lt;P&gt;I am trying to debug to check whether isr has come up or not, while loop is executing once.but going to default isr.any suggestion how to check interrupt is running or not .&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 13:17:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1828510#M33001</guid>
      <dc:creator>Ashish4525</dc:creator>
      <dc:date>2024-03-14T13:17:34Z</dc:date>
    </item>
    <item>
      <title>Re: Create a delay in s32k118 using gpt start timer</title>
      <link>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1828867#M33013</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225256"&gt;@Ashish4525&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can place a breakpoint inside your interrupt handler to confirm it is indeed running. For example, if you flash the &lt;EM&gt;lpit_periodic_interrupt_s32k118&lt;/EM&gt; example, you can place the breakpoint inside&amp;nbsp;&lt;STRONG&gt;LPIT_ISR&lt;/STRONG&gt; and confirm the isr is active:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1710456322958.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268531i4E15AA955023F94F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1710456322958.png" alt="Julin_AragnM_0-1710456322958.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_0-1710456322958.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_1-1710456399381.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268533iFB6F0503D87509C7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_1-1710456399381.png" alt="Julin_AragnM_1-1710456399381.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_1-1710456399381.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 22:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Create-a-delay-in-s32k118-using-gpt-start-timer/m-p/1828867#M33013</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-03-14T22:47:04Z</dc:date>
    </item>
  </channel>
</rss>