<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックPin configuration tool not generating all GPIO pins</title>
    <link>https://community.nxp.com/t5/S32K/Pin-configuration-tool-not-generating-all-GPIO-pins/m-p/1827331#M32923</link>
    <description>&lt;P&gt;I have configured the GPIO pins, but found that not all GPIO pins listed in generated code.&lt;/P&gt;&lt;P&gt;Siul2_Port_Ip_Cfg.h does not show few pins in the list.&lt;/P&gt;&lt;P&gt;One observation is that in&amp;nbsp;Tspc_Port_Ip_Types.h I can see below line for one of such pin. Does this tell this pin is configured as ADC?&lt;/P&gt;&lt;P&gt;#define PTC11_OBE (uint64_t)(1ULL &amp;lt;&amp;lt; 17) /* TSPC_ADC0 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 13 Mar 2024 15:53:10 GMT</pubDate>
    <dc:creator>anilsp31PA</dc:creator>
    <dc:date>2024-03-13T15:53:10Z</dc:date>
    <item>
      <title>Pin configuration tool not generating all GPIO pins</title>
      <link>https://community.nxp.com/t5/S32K/Pin-configuration-tool-not-generating-all-GPIO-pins/m-p/1827331#M32923</link>
      <description>&lt;P&gt;I have configured the GPIO pins, but found that not all GPIO pins listed in generated code.&lt;/P&gt;&lt;P&gt;Siul2_Port_Ip_Cfg.h does not show few pins in the list.&lt;/P&gt;&lt;P&gt;One observation is that in&amp;nbsp;Tspc_Port_Ip_Types.h I can see below line for one of such pin. Does this tell this pin is configured as ADC?&lt;/P&gt;&lt;P&gt;#define PTC11_OBE (uint64_t)(1ULL &amp;lt;&amp;lt; 17) /* TSPC_ADC0 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 15:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Pin-configuration-tool-not-generating-all-GPIO-pins/m-p/1827331#M32923</guid>
      <dc:creator>anilsp31PA</dc:creator>
      <dc:date>2024-03-13T15:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: Pin configuration tool not generating all GPIO pins</title>
      <link>https://community.nxp.com/t5/S32K/Pin-configuration-tool-not-generating-all-GPIO-pins/m-p/1828427#M32994</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;could be fine you show your setting and which pin is missing. I think a pins configured in Pins tool would appears within config structure in&amp;nbsp;Siul2_Port_Ip_Cfg.c, unless pin does not require any SIUL configuration.&lt;BR /&gt;&lt;SPAN&gt;Siul2_Port_Ip_Cfg.h includes just config structure declaration and macro for number of configured pins.&lt;/SPAN&gt;&amp;nbsp;&lt;BR /&gt;Pins using ADC function does not require SIUL setting.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 11:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Pin-configuration-tool-not-generating-all-GPIO-pins/m-p/1828427#M32994</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-03-14T11:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: Pin configuration tool not generating all GPIO pins</title>
      <link>https://community.nxp.com/t5/S32K/Pin-configuration-tool-not-generating-all-GPIO-pins/m-p/1833137#M33317</link>
      <description>&lt;P&gt;This issue is resolved. There were duplicate Labels/Identifiers present in the Pins configurations which may have caused these issues. I have corrected the duplicates and problem is resolved.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 17:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Pin-configuration-tool-not-generating-all-GPIO-pins/m-p/1833137#M33317</guid>
      <dc:creator>anilsp31PA</dc:creator>
      <dc:date>2024-03-21T17:57:50Z</dc:date>
    </item>
  </channel>
</rss>