<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CMU_FC destructive reset configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1826992#M32898</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228277"&gt;@FabioG&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Based on the latest update, the diagrams should be fixed in the next RM release.&lt;/P&gt;
&lt;P&gt;Both FLL and FHH can generate either an interrupt or reset. The destructive reset is bond with the asynchronous mode, and the synchronous mode only generate the interrupt.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Wed, 13 Mar 2024 08:56:08 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2024-03-13T08:56:08Z</dc:date>
    <item>
      <title>CMU_FC destructive reset configuration</title>
      <link>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1824529#M32729</link>
      <description>&lt;P&gt;Hi There,&lt;/P&gt;&lt;P&gt;1) I looking for configuring CMU_FC peripheral (Chapter 54). Revision 8 of reference manual.&lt;/P&gt;&lt;P&gt;There no explicit reference (I don't find it ...) about setting destructive reset, but in logic network at Chapter 24, par 8 "Clock Monitoring, page 960 "Figure 115. Frequency checking (FC) instances"&amp;nbsp; seems that to enable destructive reset we have to enable asyncronous interrupts FHHAIE and FLLAIE as shown for FC4,5,3 is it true ?&lt;/P&gt;&lt;P&gt;2)And why for fc0 and Fc6, in order&amp;nbsp; to enable destructive reset is activated FHHIE (Syncronous Upper threshold!! ) on the LOWER threshold path , and&amp;nbsp; for the interrupt activation&amp;nbsp; &amp;nbsp;is set FLLAIE (Lower Asyncronous)for the&amp;nbsp; UPPER threshold path&amp;nbsp; ? is it a mistake or a feature ? (see attached file)&lt;/P&gt;&lt;P&gt;2) in revision 5 of manual there was not present FC6 (CM7_CORE_CLK). what is the difference with FC3(CORE_CLK) ?&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;</description>
      <pubDate>Sat, 09 Mar 2024 10:34:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1824529#M32729</guid>
      <dc:creator>FabioG</dc:creator>
      <dc:date>2024-03-09T10:34:39Z</dc:date>
    </item>
    <item>
      <title>Re: CMU_FC destructive reset configuration</title>
      <link>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1826127#M32840</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228277"&gt;@FabioG&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1.&lt;/P&gt;
&lt;P&gt;This is under an internal discussion at the moment.&lt;/P&gt;
&lt;P&gt;2.&lt;/P&gt;
&lt;P&gt;FC_6 is available on S32K388 only.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1710242001591.png" style="width: 568px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267815i80C043E263145F00/image-dimensions/568x424?v=v2" width="568" height="424" role="button" title="danielmartynek_0-1710242001591.png" alt="danielmartynek_0-1710242001591.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1710242001591.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 11:14:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1826127#M32840</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-03-12T11:14:03Z</dc:date>
    </item>
    <item>
      <title>Re: CMU_FC destructive reset configuration</title>
      <link>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1826219#M32846</link>
      <description>&lt;P&gt;Regarding point 1: in order to checkCMU_FC&amp;nbsp; Distructive reset, what I need to configure in CMU_FC?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 13:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1826219#M32846</guid>
      <dc:creator>FabioG</dc:creator>
      <dc:date>2024-03-12T13:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: CMU_FC destructive reset configuration</title>
      <link>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1826992#M32898</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228277"&gt;@FabioG&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Based on the latest update, the diagrams should be fixed in the next RM release.&lt;/P&gt;
&lt;P&gt;Both FLL and FHH can generate either an interrupt or reset. The destructive reset is bond with the asynchronous mode, and the synchronous mode only generate the interrupt.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 08:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CMU-FC-destructive-reset-configuration/m-p/1826992#M32898</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-03-13T08:56:08Z</dc:date>
    </item>
  </channel>
</rss>