<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to integrate SCST library with existing code? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-integrate-SCST-library-with-existing-code/m-p/835073#M3288</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in this case, it would be better to create a ticket:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://nxpcommunity.force.com/community/CommunityContextPage" title="http://nxpcommunity.force.com/community/CommunityContextPage"&gt;http://nxpcommunity.force.com/community/CommunityContextPage&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Dec 2018 09:52:54 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2018-12-11T09:52:54Z</dc:date>
    <item>
      <title>How to integrate SCST library with existing code?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-integrate-SCST-library-with-existing-code/m-p/835072#M3287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to integrate the SCST library into our existing project.&lt;/P&gt;&lt;P&gt;The project is designed to run on a custom board with the S32K144 controller.&lt;/P&gt;&lt;P&gt;The project is built using GHS Compiler for ARM v2017.5.4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I execute the core self tests using the m4_scst_execute_core_tests() function,&amp;nbsp;the function returns with&amp;nbsp;M4_SCST_WRONG_RANGE.&amp;nbsp;After executing a few lines of code following the&amp;nbsp;&lt;SPAN&gt;m4_scst_execute_core_tests()&amp;nbsp; function call&amp;nbsp;I&amp;nbsp;&lt;/SPAN&gt;get a hard fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to execute the scst example&amp;nbsp;code on our custom board without issue. I get the above results only after integrating with our existing project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know how to debug this issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2018 13:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-integrate-SCST-library-with-existing-code/m-p/835072#M3287</guid>
      <dc:creator>sahyadriholagun</dc:creator>
      <dc:date>2018-12-05T13:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: How to integrate SCST library with existing code?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-integrate-SCST-library-with-existing-code/m-p/835073#M3288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in this case, it would be better to create a ticket:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://nxpcommunity.force.com/community/CommunityContextPage" title="http://nxpcommunity.force.com/community/CommunityContextPage"&gt;http://nxpcommunity.force.com/community/CommunityContextPage&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2018 09:52:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-integrate-SCST-library-with-existing-code/m-p/835073#M3288</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2018-12-11T09:52:54Z</dc:date>
    </item>
  </channel>
</rss>