<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックTwo CS in SPI0 line</title>
    <link>https://community.nxp.com/t5/S32K/Two-CS-in-SPI0-line/m-p/1826482#M32856</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;am using "FS32K148UJT0VLUT" and wanted to connect Two ADC's for SPI0 with different CS. SPI0_CS1, SPI0_CS0. Does it work?&lt;/P&gt;</description>
    <pubDate>Tue, 12 Mar 2024 18:01:19 GMT</pubDate>
    <dc:creator>manojkumar_123</dc:creator>
    <dc:date>2024-03-12T18:01:19Z</dc:date>
    <item>
      <title>Two CS in SPI0 line</title>
      <link>https://community.nxp.com/t5/S32K/Two-CS-in-SPI0-line/m-p/1826482#M32856</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;am using "FS32K148UJT0VLUT" and wanted to connect Two ADC's for SPI0 with different CS. SPI0_CS1, SPI0_CS0. Does it work?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 18:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Two-CS-in-SPI0-line/m-p/1826482#M32856</guid>
      <dc:creator>manojkumar_123</dc:creator>
      <dc:date>2024-03-12T18:01:19Z</dc:date>
    </item>
    <item>
      <title>Re: Two CS in SPI0 line</title>
      <link>https://community.nxp.com/t5/S32K/Two-CS-in-SPI0-line/m-p/1826854#M32886</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Do you want to select a different salve via SPI0_CSx? Yes, you can select different slaves through SPI0_CS0~SPI0_CS3.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Multiple slave devices are selected using individual slave select (SS) lines.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/268037i64ED72BBBD343667/image-size/large?v=v2&amp;amp;px=999" role="button" title="Multiple slave devices are selected using individual slave select (SS) lines.png" alt="Multiple slave devices are selected using individual slave select (SS) lines.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 06:36:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Two-CS-in-SPI0-line/m-p/1826854#M32886</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-03-13T06:36:58Z</dc:date>
    </item>
  </channel>
</rss>